Hello,I have encountered a problem:Using JTAG mode for S32K148 download and debugging in Keil IDE will result in an error message."No Cortex-M Device found in JTAG chain".Without changing the hardware environment,I have made the following attempts but have been unable to resolve them, so the preliminary conclusion is that there is a problem between Keil and the MCU。
Attempt 1:Keil+SWD is ok, IAR+SWD/JTAG are both ok, S32DS+SWD/JTAG are both ok.
Attempt 2:I have downgraded the keil dfp pack package version from 1.5.0 to 1.3.0,but none of them worked.
Attempt 3:I replaced Keil's J-Link driver “JLinkARM.dll”, but it still doesn't work
Attempt 4:I can download it separately using the JTAG mode of the Segger J-Flash tool.
Attempt 5:I have also tried changing Keil versions, 5.34 and 5.39, but none of them worked.
So I don't know where the problem is, I suspect it's an internal issue with Keil or an incompatibility issue between Keil and S32K series chips in JTAG mode.
Please help confirm ,thanks.The error report photo is attached.
Hi @Guo_Jing,
Since it works with IAR, S32DS, J-Flash, please contact KEIL support.
Thank you,
BR, Daniel
Unfortunately, it's been 2 weeks and Keil Support hasn't replied .
Can you please pay attention to this issue?