we have a product with UJA1169TK which only support CAN HS, not support CAN FD, this product will send message to product B which support CAN FD, our product will report error frame in can network, because it doesn't support CAN FD, is there any method to stop reporting error frame for our product?
I have a propose, let out product enable the CAN transmitter(TXD) and disable the receiver(RXD), I am not sure it's applicable, it's opposite with CAN Listen-only mode which disable the CAN transmitter(TXD) and enable the receiver(RXD)
so I need your help, thanks!
Solved! Go to Solution.
Hi,
CAN FD node should be able to receive CAN 2.0 message, so your CAN2.0 node should nto get error for this. But correct for receiving CAN FD message, for this CAN2.0 node send error frame.
The scenario you outlined is not possible. For transmitting message FlexCAN have to read it back so CAN receiver have to be active too.
BR, Petr
Hi,
CAN FD node should be able to receive CAN 2.0 message, so your CAN2.0 node should nto get error for this. But correct for receiving CAN FD message, for this CAN2.0 node send error frame.
The scenario you outlined is not possible. For transmitting message FlexCAN have to read it back so CAN receiver have to be active too.
BR, Petr