In S32K1XX why VoL & VoH details are not provided in datasheet?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In S32K1XX why VoL & VoH details are not provided in datasheet?

1,634 Views
srikanthkala
Contributor III

Hello Team,

As i heard that if the internal circuitry of I/O is open collector the VoL & VoH were dependent on the external interfaced resistors consumption.

Kindly share info if you have any including the details of VoL & VoH

Thanks 

Srikanth.K

8 Replies

1,404 Views
srikanthkala
Contributor III

Hello Team,

Thanks for your support, i am very satisfied with your support, i have small query in the same topic,

In the above minimum currents of I/O are like 5mA, 20mA, 14.0mA based on the operation of I/O.

In my case we are using for SPI communication which can actually source up to 10 mA (i.e slave). In which mode and in which case the controller SPI(i.e. S32k) configuration has maximum currents in all cases of MISO, MOSI,SCLK, CS,

What are the maximum source and sink currents if i operate for SPI communication,

Thanks

Srikanth kala

Valeo

0 Kudos

1,404 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Srikanth Kala,

Section 6.5.2 in the S32K1xx DS, rev.9 provides LPSPI electrical specifications.

As you can see, the measurement were taken with DSE = 1.

pastedImage_1.png

Only pins that are specified as GPIO_HD (PAD TYPE) in S32K1xx_IO_Signal_Description_Input_Multiplexing.xlsx can be set to High drive strength (PORT_PCRn_DSE = 1).

pastedImage_4.png

pastedImage_1.png

Regards,

Daniel

0 Kudos

1,404 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,
There are VoL, VoH specification in the DS, please have a look at Table 12 (DC electrical specifications at 5.0 V Range).
For example, VoH = VDD – 0.8V, when a GPIO pin is loaded with 5mA (DSE = 0) or 20mA (DSE = 1 (GPIO-HD pins only)).

Regards,
Daniel

0 Kudos

1,404 Views
srikanthkala
Contributor III

Hello Diana,

Thanks for your reply 

I have gone through the datasheet, Table 12 consists of only below parameters, but i couldn't see anything related to VoH and VoL

@S32K1XXX

pastedImage_1.png

Below is the datasheet i am referring to

pastedImage_2.png

Thanks,

Srikanth.K

0 Kudos

1,404 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Please refer to the up-to-date version S32K1xx DS rev.9.

Thank you,

Regards,

Daniel

1,404 Views
srikanthkala
Contributor III

Hello Team,

Please provide Voh range , from datasheet i can take Voh= 5.5-0.8 => 4.7 V as Voh max but Voh min value  ir required to justify my interface

Thanks,

Srikanth

0 Kudos

1,404 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

V_OH is equal to VDD if the pin is not loaded externally.

But if loaded, the voltage drops to VDD - 0.8V at 5mA (PCR_DSE = 0), for example.

pastedImage_1.png

Regards,

Daniel

1,404 Views
srikanthkala
Contributor III

Hello Diana,

Just now checked new revision,

Thanks for your kind support.

Regards,

Srikanth.K

0 Kudos