I2C interface in S32K148 EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C interface in S32K148 EVB

ソリューションへジャンプ
2,816件の閲覧回数
sgp_118
Contributor II

Hi All,

I want to test I2C functionality in S32K148 EVB Rev B board. Could you please help in pointing out which peripheral(s) on the board can be used for testing the same?

Also are there any links for application code which are written specifically for this EVB?

Regards,

Guru

タグ(1)
0 件の賞賛
返信
1 解決策
2,737件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Guru,

Please download the latest S32 Design Studio for ARM 2.2 – Windows/Linux(REV 2.2), then you can refer these lpi2c examples of S32K148.

lpi2c_master_s32k148.png

LPI2C1.png

You may need to test the I2C functionality by using two boards or logic analyzer.

You can download Schematics and User Manual of  S32K148EVB from here.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,737件の閲覧回数
sgp_118
Contributor II

Thanks, Robin

0 件の賞賛
返信
2,738件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Guru,

Please download the latest S32 Design Studio for ARM 2.2 – Windows/Linux(REV 2.2), then you can refer these lpi2c examples of S32K148.

lpi2c_master_s32k148.png

LPI2C1.png

You may need to test the I2C functionality by using two boards or logic analyzer.

You can download Schematics and User Manual of  S32K148EVB from here.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 件の賞賛
返信
2,469件の閲覧回数
pjain_123
Contributor I

@Robin_Shen I installed the S32DS on my Linux system but I am not able to view all the I2C example codes (like lp12c_master_s32k148 example code). Could you please direct me how to get all the example codes? I tried looking for SDKs but the S32DS IDE informs me that it's upto date.Screenshot from 2021-07-20 17_53_18.png

0 件の賞賛
返信
2,461件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi pjain_123,

Please install: S32 Design Studio for ARM 2.2 - Update 1 available

Best Regards,
Robin

0 件の賞賛
返信
2,452件の閲覧回数
pjain_123
Contributor I

@Robin_Shen I still don't see the "S32K1xx development package", "S32K1xx SDK 3.0.3 pakage" after the update. I am using Ubuntu 14.04LTS. Is there any way I could get the update? PFA the screenshot of my S32DS Extension and Updates window


pjain_123_0-1626846464652.png

 

 

0 件の賞賛
返信