I2C interface in S32K148 EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C interface in S32K148 EVB

Jump to solution
2,521 Views
sgp_118
Contributor II

Hi All,

I want to test I2C functionality in S32K148 EVB Rev B board. Could you please help in pointing out which peripheral(s) on the board can be used for testing the same?

Also are there any links for application code which are written specifically for this EVB?

Regards,

Guru

Tags (1)
0 Kudos
Reply
1 Solution
2,442 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Guru,

Please download the latest S32 Design Studio for ARM 2.2 – Windows/Linux(REV 2.2), then you can refer these lpi2c examples of S32K148.

lpi2c_master_s32k148.png

LPI2C1.png

You may need to test the I2C functionality by using two boards or logic analyzer.

You can download Schematics and User Manual of  S32K148EVB from here.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
5 Replies
2,442 Views
sgp_118
Contributor II

Thanks, Robin

0 Kudos
Reply
2,443 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Guru,

Please download the latest S32 Design Studio for ARM 2.2 – Windows/Linux(REV 2.2), then you can refer these lpi2c examples of S32K148.

lpi2c_master_s32k148.png

LPI2C1.png

You may need to test the I2C functionality by using two boards or logic analyzer.

You can download Schematics and User Manual of  S32K148EVB from here.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 Kudos
Reply
2,174 Views
pjain_123
Contributor I

@Robin_Shen I installed the S32DS on my Linux system but I am not able to view all the I2C example codes (like lp12c_master_s32k148 example code). Could you please direct me how to get all the example codes? I tried looking for SDKs but the S32DS IDE informs me that it's upto date.Screenshot from 2021-07-20 17_53_18.png

0 Kudos
Reply
2,166 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi pjain_123,

Please install: S32 Design Studio for ARM 2.2 - Update 1 available

Best Regards,
Robin

0 Kudos
Reply
2,157 Views
pjain_123
Contributor I

@Robin_Shen I still don't see the "S32K1xx development package", "S32K1xx SDK 3.0.3 pakage" after the update. I am using Ubuntu 14.04LTS. Is there any way I could get the update? PFA the screenshot of my S32DS Extension and Updates window


pjain_123_0-1626846464652.png

 

 

0 Kudos
Reply