FS26 Installation failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 Installation failure

506 Views
Lica
Contributor II

FS26 SBC used by S32K344 MCU, installing FS26 plugin in S32 Design Studio for S32 Plaform does not install successfully, I can import FS26 demo, but the most critical problem is that the Sbc component cannot be found in the MCAL GUI after installation.

In addition, I have paid attention to the details of version matching and closing the anti-virus software during the installation process.

1.png2.png3.png

The following is my RTD, FS26 installation package version, thanks for your help.

4.png6.png7.png

0 Kudos
3 Replies

495 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Lica,

If you use S32DS v3.4 IDE.

Please install FS26_4.4_1.0.0_CD02_DS_updatesite_D2303.zip with SW32K3_RTD_4.4_2.0.3_DS_updatesite_D2302.zip.

Or install FS26_4.4_1.0.0_RTM_DS_updatesite_D2209.zip with SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip.

Automotive SW - SBC PMIC - Real Time Drivers (Example Code).png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos

491 Views
Lica
Contributor II
Thank you for your help.
I installed SW32K3_RTD_4.4_2.0.2_DS_updatesite_D2211
The corresponding driver package was not found。
I failed to install both SW32K3_RTD_4.4_2.0.3_DS_updatesite_D2302.zip and SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip in the screenshot
0 Kudos

492 Views
Lica
Contributor II
I installed SW32K3_RTD_4.4_2.0.2_DS_updatesite_D2211
The corresponding driver package was not found
0 Kudos