Hi ,
I am using a S32K116 micro controller for my application. Currently am using PTC6 as LPUART1 receive pin and PTC7 as LPUART1 Transmit pin.
I need to enable the High Drive Strength for Tx pin (PTC7).
I have used below configuartion for enabling High Drive strength .
Is this correct? If it wrong can anyone direct to me the correct configurations ?
Thanks,
Satheesh
Hello Satheesh,
Your implementation is correct.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct"button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------