Does NXP have a similar safeTlib(Infineon AURIX)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does NXP have a similar safeTlib(Infineon AURIX)

698 Views
jingfang
Contributor IV

Use S32K144+FS84 to achieve ASIL B instead of Infineon.

Basing on the safeTlib code package,realizes the detection of AURIX hardware safety mechanism by using AUTOSAR multi-core operating system,which makes the motor controller software meet the functional safety requirements.

Does NXP have a similar safeTlib or make sure ASIL B(include software and hardware)?

0 Kudos
1 Reply

674 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

NXP RTD is developed as per ISO26262 standard and allows integration into safety applications up to ASIL-D (i.e. highest safety integrity level)

FS84 is developed in compliance with the ISO 26262 standard and is qualified according to AEC-Q100 requirements.

Best Regards,

Nam

0 Kudos