Building S32K344 project in S32DS3.4 take more than 5min ?

取消
显示结果 
搜索替代 
您的意思是: 

Building S32K344 project in S32DS3.4 take more than 5min ?

287 次查看
phidiawang
Contributor III

Hi,

I built  a S32K344 project in S32DS3.4,and it took me for more than 5min.Can I speed up it ?thanks.

微信图片_20220104134435.png

标记 (1)
0 项奖励
3 回复数

264 次查看
phidiawang
Contributor III

Senlent:

thanks. I modifed that setting as you said,but it is still very slow.

0 项奖励

253 次查看
Senlent
NXP Employee
NXP Employee

Hi@phidiawang

    I have also encountered a situation that can reduce the build-time,which is disconnecting the network,because the S32 DS background update tasks will increase the burden of the CPU, maybe you can try this method is effective to you or not.

BR!

     Jim,

0 项奖励

275 次查看
Senlent
NXP Employee
NXP Employee

Hi@phidiawang

There some tips may help you speed up your build time.

 

Fist, you can close the unused project ,as I can see that you opened many unused projects,and then try to clean the project you using,then build it again.

 

Second,try to expand the max heap size of S32 DS.

please try to click below link for details.

https://community.nxp.com/t5/S32K/How-to-expand-the-max-heap-size-of-s32ds/td-p/1379575 

BR!

     Jim,

 

0 项奖励