关于K344 FlexIO模拟6路SENT接口参考例程

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

关于K344 FlexIO模拟6路SENT接口参考例程

1,109件の閲覧回数
zhijian
Contributor I

hi,

       NXP是否有针对FlexIO模拟多通道SENT接口参考方案及配置参考例程(DMA方式),我们用到一个4+2的角度传感器(SENT接口),目前使用DMA配置一路SENT ,SNET信号能正确捕捉; 配置2路SNET后,2路SNET数据都为异常,1,2两路数据有会有交叉更新。针对FlexIO模拟多通道SENT(DMA方式)需要怎么配置?谢谢!

0 件の賞賛
返信
4 返答(返信)

1,080件の閲覧回数
JoaquinL
NXP Employee
NXP Employee

Hi,

The sample project has been sent to the customer through FAE, and this post can be closed.

BR, Joaquin

0 件の賞賛
返信

998件の閲覧回数
abc1258
Contributor I
Hello,@ JoaquinL
I also need this routine, could you share a copy with me? Thank you
0 件の賞賛
返信

987件の閲覧回数
JoaquinL
NXP Employee
NXP Employee

Hi,

The K3 RTD 3.0.0 was released recently. You can try the example project of SENT driver in RTD.

This post was only for old version RTD and it may not work now.

Thank you!

BR, Joaquin

0 件の賞賛
返信

969件の閲覧回数
abc1258
Contributor I
ok ,thanks
0 件の賞賛
返信