Example S32K344 PIT TRGMUX ADC DS3.5 RTD300

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example S32K344 PIT TRGMUX ADC DS3.5 RTD300

Example S32K344 PIT TRGMUX ADC DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of 
 configure TRGMUX to select triggers for staring Normal/Injected chain conversion.

Select PIT0_Ch0 as the hardware trigger source of ADC1_Ch34 & Ch48 via TRGMUX and two LEDs to show the trigger Sequence.

ADC1_Ch34 is connected to board's potentiometer,Ch38 is bandgap channel.

 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-Q257
* MCU: S32K344
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: OpenSDA
* Target: internal_FLASH
********************************************************************************

附件
无评分
版本历史
最后更新:
‎11-21-2023 07:28 PM
更新人: