Example S32K344 PIT TRGMUX ADC DS3.5 RTD300

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example S32K344 PIT TRGMUX ADC DS3.5 RTD300

Example S32K344 PIT TRGMUX ADC DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of 
 configure TRGMUX to select triggers for staring Normal/Injected chain conversion.

Select PIT0_Ch0 as the hardware trigger source of ADC1_Ch34 & Ch48 via TRGMUX and two LEDs to show the trigger Sequence.

ADC1_Ch34 is connected to board's potentiometer,Ch38 is bandgap channel.

 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-Q257
* MCU: S32K344
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: OpenSDA
* Target: internal_FLASH
********************************************************************************

添付
評価なし
バージョン履歴
最終更新日:
‎11-21-2023 07:28 PM
更新者: