Example S32K144 RTC VLPS

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

Example S32K144 RTC VLPS

評価なし

Example S32K144 RTC VLPS

********************************************************************************************************************************************
Detailed Description:
This example shows use of RTC in VLPS mode.
The MCU is put into the VLPS mode (Sleep-On-Exit).

RTC alarm interrupt brings it to VLPR every 3s and toggles BLUE LED (PTD0).
Since it works in the Sleep-On-Exit mode, after the ISR, the MCU goes to VLPS again without calling the WFI instruction.
When BTN0 (S32K144 EVB) is pressed, the power mode switch from VLPS to VLPR and other way round.
Interrupt is triggered on rising edge (PTC12), filtered by digital filter (clocked from LPO).
In VLPR, RTC seconds interrupt is enabled as well and toggles RED LED (PTD15) in the ISR.
RTC_CLKOUT (1Hz) and CLKOUT (bus_clk) can be monitored at PTD13 and PTD14 respectively.
CLKOUT is not available in VLPS.
The MCU needs to be power-cycled and run stand-alone.
--------------------------------------------------------------------------------------------------------------------------------------------------------------------
Test HW: S32K144EVB-Q100
MCU: S32K 0N57U
Debugger: S32DS_ARM_2.2, OpenSDA
Target: internal_FLASH
********************************************************************************************************************************************

タグ(3)
添付
コメント

Hi Daniel,

I found an issue when I follow your example:

pastedImage_1.png

You set SCG->SIRCCSR[LK] = 0 at position 24, but when I check in datasheet LK is in 23.

Should I use bit 23 or 24 right here?

Hi Nhuan,

Thank you, it has been updated.

Regards,

Daniel

バージョン履歴
改訂 #:
1/1
最終更新日:
‎10-22-2018 06:35 AM
更新者: