Example MCAL S32K312 PWM ICU using EMIOS DS3.5 RTD300

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MCAL S32K312 PWM ICU using EMIOS DS3.5 RTD300

Example MCAL S32K312 PWM ICU using EMIOS DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
ICU & PWM MCAL Driver for the S32K3xx MCU.

This example uses the custom IRQ.


The example uses:--

EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM
EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty

Dinesh_Guleria_0-1733220239428.png

 


 

Dinesh_Guleria_1-1733220247864.png

 



Result :--

Dinesh_Guleria_2-1733220259942.png

 


 




 ------------------------------------------------------------------------------
* Test HW: S32K3X2EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

附件
无评分
版本历史
最后更新:
‎12-10-2024 11:41 PM
更新人: