Is there any FlexRay driver (test code) for S32G?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there any FlexRay driver (test code) for S32G?

1,502 次查看
Wanyj
Contributor I

Hi:

    I want to know,How can I verify that FlexRay is working properly on the S32G and can I just monitor it with software without a FlexRay transceiver

0 项奖励
回复
7 回复数

1,474 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @Wanyj 

The examples provided under S32 Design Studio, are meant to be used as board to board, so you need to connect to board, each with one individual or unique node example. You can verify the examples by debugging them.

Miguel04_0-1699295474079.png

Best Regards, Miguel.

 

0 项奖励
回复

1,443 次查看
Wanyj
Contributor I

Hi

First of all thank you for sharing, I also want to ask if I run this sample code where I can observe anything? How to know that the data has been successfully sent and received.

Best Regards, Wanyj

0 项奖励
回复

1,413 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @Wanyj 

I'm happy to help you. You can verify the transmission by pausing the debug session and review the values of the RecieveArray or connect an oscilloscope to the pins to see the signal.

I also recommend you to look into the description.txt file on the example, here you will find a lot of details regarding the example, such as the supported hardware and the application software functionality.

Miguel04_0-1699903943441.png

 

Let me know if you have a question.

Best Regards, Miguel.

0 项奖励
回复

1,400 次查看
Wanyj
Contributor I

Hi,Miguel04 

  •       I'm using the example from S32G LLCE 1_0_5,But now it fails to compile, it indicates that the SchM_Fr_43_LLCE.h file is missing, when I added this file, it also indicates that the definition of some functions is missing, I found that these functions are contained in SchM_Fr_43_LLCE.h.

  •     May I ask if the LLCE sample code is not available? Or there is something wrong with my method of use, and I have not found the exact operation steps on the official website. Please kindly answer it for me. Thank you for your help!   
  •     As for your kindest regards,I hope you can answer my question
0 项奖励
回复

1,391 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @Wanyj 

I'll look into it.

Can you share images for all the errors you are getting please?

Best Regards, Miguel.

0 项奖励
回复

1,382 次查看
Wanyj
Contributor I

Hi,Miguel04

    I am using the example shown below, however, it will have a compilation error, please take a look at the problem?

Wanyj_0-1700010809812.png

Wanyj_1-1700010853077.png

     These undefined functions exist in this.h file, and I added the dependency path myself, because at first it reported an error that the.h file could not be found.

Wanyj_2-1700011051150.png

     Hope to get your answer.Best Regards, Miguel.

 

0 项奖励
回复

1,320 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @Wanyj 

It seems that the case is being followed under the next post.

FlexRay test of S32G-VNP-RDB2

Do you prefer we use information from that post and follow up or the support can continue on the other thread?

Best Regards, Miguel.

0 项奖励
回复