Install new apps like docker which takes more size (~100mb) on S32G VNP RDB2 since we have only 45mb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Install new apps like docker which takes more size (~100mb) on S32G VNP RDB2 since we have only 45mb

234 Views
iamramcharan
Contributor II

Install new apps like docker which takes more size (~100mb) on S32G VNP RDB2 since we have only 45mb in /dev/

 

 

s32g274ardb2:/# df -H
Filesystem Size Used Avail Use% Mounted on
/dev/root 529M 444M 45M 91% /
devtmpfs 1.7G 0 1.7G 0% /dev
tmpfs 1.8G 0 1.8G 0% /dev/shm
tmpfs 717M 18M 700M 3% /run
tmpfs 4.2M 0 4.2M 0% /sys/fs/cgroup
tmpfs 1.8G 248M 1.6G 14% /tmp
tmpfs 1.8G 168k 1.8G 1% /var/volatile
tmpfs 1.8G 0 1.8G 0% /var/volatile/tmp
tmpfs 359M 0 359M 0% /run/user/1000

Tags (3)
0 Kudos
2 Replies

214 Views
iamramcharan
Contributor II

Thanks for the response. Can we use any external disk to link to S32G board and use it ?

0 Kudos

225 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You have to decompressed the file in ubuntu or in the host the pass to S32G there is no other way.

Regards

0 Kudos