Implementing AVB/TSN in S32G-VNP-GLDBOX-3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Implementing AVB/TSN in S32G-VNP-GLDBOX-3

867 Views
minjun39
Contributor I

I want to know how to implement AVB/TSN on S32G-VNP-GLDBOX-3 I'm not sure how to connect the pins of J5,J6 in the gold box example as well and can you tell me in detail how to implement TSN??

0 Kudos
Reply
2 Replies

815 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @minjun39 

The implementation for AVB and TSN, both seems to be supported under the SJA1110 and AVB is also supported under S32G, unfortunately, since this documentations is available under NDA (for SJA1110), there is not much information or examples by our side. 

I recommend you to contact your DFAE or NXP representative, they might be able to provide you more documentation for your inquiry.

Regarding your other question.

Can you be more specific with "connect the J5 and J6 Pins"? Which connections you are trying to accomplish? The J5 pins are usually used for GPIO, ADC, SPI etc and J6 for CAN and LIN protocols.

Best Regards, Miguel.

0 Kudos
Reply

746 Views
minjun39
Contributor I

I was implementing an example using S32G-vnp-GLDBOX3.

 

Among the contents over there
Connect LLCE CAN0 to LLCE CAN1 and LLCE LIN2 (leader) to LLCE LIN3 (follower).
I am wondering if it is okay to connect [LLCE CAN0 and LLCE CAN1] and [LLCE LIN2 and LLCE LIN3] through the breadboard without connecting other ground wires and power wires in parts J5 and J6.

0 Kudos
Reply