How can the M and A cores be packaged into A burning image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can the M and A cores be packaged into A burning image

636 Views
jianqun
Contributor II
Today we verified M7 starting from QFLASH and SD, M7 can start from QFLASH and SD alone,Core A now boots from an SD card ,but the dip switch for starting from QFLASH and SD is different on RDB board,How do we get M and A to start at the same time, or do we start M and then pull up A,How do we package both M and A cores into the same image file
 
0 Kudos
2 Replies

621 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello jianqun,

You can't burn in the same package, you can create a new repository in yocto to create all the core M stuff and burn your S32, then run the M0.

 

Regards

 

0 Kudos

610 Views
jianqun
Contributor II

There are detailed documentation, our development environment is S32DS

0 Kudos