Boot m7_0 failed on S32G-VNP-RDB2 followed AN13750.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Boot m7_0 failed on S32G-VNP-RDB2 followed AN13750.

469 次查看
chengpei
Contributor III

Hello,

I want to boot A53 from m7_0 on S32G-VNP-RDB2, and I followed the steps in this document <AN13750 Enabling Multicore Application on S32G2>.

After I flashed my binaries to my board, the m7_0 did not even started, as the lauterbach said "running(reset)", which means the core did not start.

chengpei_2-1700753384663.png

Is there something wrong with this "s32g2xx_hse_fw_0.1.0_1.0.5_pb220413.bin.pink"?

Can you give me a blob binary which can boot m7_0 and then boots A53 successfully? 

My Lauterbach flashing script:

chengpei_1-1700753365275.png

My IVT configuration:

chengpei_0-1700752906563.png

Below is my blob.

0 项奖励
回复
1 回复

455 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Which Bootloader version are you using? Which BSP version are you using? Have you confirmed that your BSP image is working as expected after the required modifications?

Have you confirmed that your HSE image is working? There is a DEMOAPP for HSE that explains the required steps to enable HSE and the usage of pink and blue image.

As for HSE enabled Bootloader, AN13750 details modifications required under the Bootloader source, have you applied the required modifications to the specified source files?

Please, let us know.

0 项奖励
回复