Can't use the Processor Expert for MPC5746R or MPC5743R

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't use the Processor Expert for MPC5746R or MPC5743R

ソリューションへジャンプ
2,510件の閲覧回数
rupingliu
Contributor I

Hi,

   We found that it can't use the Processor Expert tool when we “New” a project for MPC5746R / MPC5743R in S32 Design Studio for Power Architecture 2017.R1 .

   The S32DS had been updata to "S32 Design Studio for Power Architecture 2017.R1 Update 7 ", but it was still can't find the usable SDK.

   Can someone help us to figure out it?

   Thank you !

ラベル(1)
0 件の賞賛
返信
1 解決策
2,332件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

yes, this is correct, because Processor Expert is tool for creating SDK setting. Unfortunately, SDK for MPC574xR was not released yet.

According to the SDK road map, this SDK should be released at the end of October.

Regards,

Martin

元の投稿で解決策を見る

2 返答(返信)
2,333件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

yes, this is correct, because Processor Expert is tool for creating SDK setting. Unfortunately, SDK for MPC574xR was not released yet.

According to the SDK road map, this SDK should be released at the end of October.

Regards,

Martin

2,332件の閲覧回数
rupingliu
Contributor I

Thank you very much for your answer.

0 件の賞賛
返信