The operational performance of projects compiled by S32DS keil IAR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The operational performance of projects compiled by S32DS keil IAR

ソリューションへジャンプ
406件の閲覧回数
zhangchun
Contributor III

I am optimizing an electrical engineering project and currently using S32DS for development. After optimization, the logic of the motor control part requires 30us, which cannot meet my needs.

I would like to know if using keil or IAR can improve code performance? Because I saw someone using Keil to compile results that looked a lot better from the perspective of occupied memory space

https://mp.weixin.qq.com/s?__biz=MzI0MDk0ODcxMw==&mid=2247485570&idx=1&sn=0523356c29468baed0abeffea8...

zhangchun_0-1692283357166.png

 

タグ(1)
0 件の賞賛
1 解決策
363件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

it's hard to answer if the using IAR or Keil can fix your issue - you need to test it by yourself. It is possible than Keil or IAR will be better than GNU gcc (which is free open source tool).  

 

Best way - especially in such time critical parts like motor control - is manual optimization of your code and find the way how to write it better. 

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
364件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

it's hard to answer if the using IAR or Keil can fix your issue - you need to test it by yourself. It is possible than Keil or IAR will be better than GNU gcc (which is free open source tool).  

 

Best way - especially in such time critical parts like motor control - is manual optimization of your code and find the way how to write it better. 

0 件の賞賛
359件の閲覧回数
zhangchun
Contributor III
Thank you for your reply

After experiments, the performance of the same code running on keil did not improve,

Thank you for your big suggestion. I will manually optimize the code later on
0 件の賞賛