Hi
Working in S32DS 3.5 with S32G2 and trying to add RTD 4.4 4.0.1 using the only available exe file SW32G_RTD_4.4_4.0.1_D2302 does not end but fails with the following error dialog
Did this in two workstations, same result
Solution please
Solved! Go to Solution.
Solved
It's the length of the installed directory, if exceeds 260 characters (windows limit) it fails
make it short
Solved
It's the length of the installed directory, if exceeds 260 characters (windows limit) it fails
make it short