09:43:12 **** Build of configuration Debug for project S32R41_TEF82_APP_M7_1 ****
make -j12 all
Building file: ../src/startup/Vector_Table.s
Building file: ../src/startup/startup.s
Building file: ../src/startup/system.c
Building file: ../src/ipcf_sample/ipcf_sample.c
Invoking: Standard S32DS Assembler
Invoking: Standard S32DS Assembler
arm-none-eabi-gcc "@src/startup/Vector_Table.args" -o "src/startup/Vector_Table.o" "../src/startup/Vector_Table.s"
arm-none-eabi-gcc "@src/startup/Vector_Table.args" -o "src/startup/startup.o" "../src/startup/startup.s"
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/ipcf_sample/ipcf_sample.args" -MMD -MP -MF"src/ipcf_sample/ipcf_sample.d" -MT"src/ipcf_sample/ipcf_sample.o" -o "src/ipcf_sample/ipcf_sample.o" "../src/ipcf_sample/ipcf_sample.c"
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/startup/system.args" -MMD -MP -MF"src/startup/system.d" -MT"src/startup/system.o" -o "src/startup/system.o" "../src/startup/system.c"
Building file: ../src/main.c
Building file: ../generate/src/Clock_Ip_Cfg.c
In file included from ../RTOS_S32R41/ssc/inc/Os.h:67,
from ../src/ipcf_sample/ipcf_sample.c:43:
../RTOS_S32R41/ssc/inc/Os_prop_autosar_api.h:44:17: fatal error: Os_prop.h: No such file or directory
44 | #include "Os_prop.h" /* OS Properties */
Invoking: Standard S32DS C Compiler
| ^~~~~~~~~~~
compilation terminated.
Invoking: Standard S32DS C Compiler
Building file: ../generate/src/OsIf_Cfg.c
Finished building: ../src/startup/Vector_Table.s
In file included from ../RTOS_S32R41/ssc/inc/Os_prop_autosar.h:44,
from ../RTOS_S32R41/ssc/inc/Os_prop_platform.h:45,
from ../RTOS_S32R41/ssc/inc/Os_platform_base.h:38,
from ../RTOS_S32R41/ssc/hwspec/s32r41_interrupt_router.h:26,
from ../src/startup/system.c:22:
../RTOS_S32R41/ssc/inc/Os_prop_autosar_api.h:44:17: fatal error: Os_prop.h: No such file or directory
44 | #include "Os_prop.h" /* OS Properties */
| ^~~~~~~~~~~
compilation terminated.
Finished building: ../src/startup/startup.s
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@generate/src/Clock_Ip_Cfg.args" -MMD -MP -MF"generate/src/OsIf_Cfg.d" -MT"generate/src/OsIf_Cfg.o" -o "generate/src/OsIf_Cfg.o" "../generate/src/OsIf_Cfg.c"
make: *** [src/ipcf_sample/subdir.mk:20: src/ipcf_sample/ipcf_sample.o] Error 1
arm-none-eabi-gcc "@generate/src/Clock_Ip_Cfg.args" -MMD -MP -MF"generate/src/Clock_Ip_Cfg.d" -MT"generate/src/Clock_Ip_Cfg.o" -o "generate/src/Clock_Ip_Cfg.o" "../generate/src/Clock_Ip_Cfg.c"
make: *** Waiting for unfinished jobs....
make: *** [src/startup/subdir.mk:33: src/startup/system.o] Error 1
arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"
In file included from ../RTOS_S32R41/ssc/inc/Os.h:67,
from D:/beifen/software/NXPS32DS.3.5/S32DS/software/PlatformSDK_SAF85_S32R41_2022_08/SW32R_RTD_4_4_0_9_0_D2208/BaseNXP_TS_T40D47M9I0R0/include/OsIf_Internal.h:49,
from D:/beifen/software/NXPS32DS.3.5/S32DS/software/PlatformSDK_SAF85_S32R41_2022_08/SW32R_RTD_4_4_0_9_0_D2208/BaseNXP_TS_T40D47M9I0R0/include/Mcal.h:66,
from D:/beifen/software/NXPS32DS.3.5/S32DS/software/PlatformSDK_SAF85_S32R41_2022_08/SW32R_RTD_4_4_0_9_0_D2208/BaseNXP_TS_T40D47M9I0R0/include/Devassert.h:29,
from ../RTD/include/OsIf_Cfg_TypesDef.h:54,
from ../generate/src/OsIf_Cfg.c:47:
../RTOS_S32R41/ssc/inc/Os_prop_autosar_api.h:44:17: fatal error: Os_prop.h: No such file or directory
44 | #include "Os_prop.h" /* OS Properties */
| ^~~~~~~~~~~
compilation terminated.
In file included from ../RTOS_S32R41/ssc/inc/Os.h:67,
from ../RTD/include/OsIf_Internal.h:49,
from ../RTD/include/OsIf.h:45,
from ../src/main.c:43:
../RTOS_S32R41/ssc/inc/Os_prop_autosar_api.h:44:17: fatal error: Os_prop.h: No such file or directory
44 | #include "Os_prop.h" /* OS Properties */
| ^~~~~~~~~~~
compilation terminated.
In file included from ../RTOS_S32R41/ssc/inc/Os.h:67,
from D:/beifen/software/NXPS32DS.3.5/S32DS/software/PlatformSDK_SAF85_S32R41_2022_08/SW32R_RTD_4_4_0_9_0_D2208/BaseNXP_TS_T40D47M9I0R0/include/OsIf_Internal.h:49,
from D:/beifen/software/NXPS32DS.3.5/S32DS/software/PlatformSDK_SAF85_S32R41_2022_08/SW32R_RTD_4_4_0_9_0_D2208/BaseNXP_TS_T40D47M9I0R0/include/Mcal.h:66,
from ../RTD/include/Clock_Ip_Specific.h:50,
from ../RTD/include/Clock_Ip_Private.h:55,
from ../generate/src/Clock_Ip_Cfg.c:48:
../RTOS_S32R41/ssc/inc/Os_prop_autosar_api.h:44:17: fatal error: Os_prop.h: No such file or directory
44 | #include "Os_prop.h" /* OS Properties */
| ^~~~~~~~~~~
compilation terminated.
make: *** [generate/src/subdir.mk:26: generate/src/OsIf_Cfg.o] Error 1
make: *** [src/subdir.mk:20: src/main.o] Error 1
make: *** [generate/src/subdir.mk:26: generate/src/Clock_Ip_Cfg.o] Error 1
"make -j12 all" terminated with exit code 2. Build might be incomplete.
09:43:16 Build Failed. 11 errors, 0 warnings. (took 3s.646ms)
No file is generated when this key is pressed
The os configuration file for this project is not generated
The problem has been solved.This is a problem with the executable files in the version.I just replaced the 0.8 version with the 0.9 version.And I dont know why the sg.exe with 0.8 version execution error.Prompt information in the fourth picture.
Thanks for your reply.
T
Hi @RanDong ,
Great that you were able to get the solution for the issue. Happy coding.
Best regards,
- Mehul
I have one more question:The RTOS S32R41 0.9.0 version Can't install.
Can you help me with that.
Thanks.
Hi, @RanDong ,
Please can you provide more information and what explanation in more detail. Also please can you provide the workspace log from:
S32DS workspace: C:\Users\Public\[workspace_name]\.metadata
( or where the workspace is located please can you provide the log folder)
Also, it seems you may be steps missed following some particular step and creating the issue. Please can you read the description for the project or readme file and follow the step mention in it
Thank you. Kind regards.
- Mehul Patel