Hi,
I came across this post when trying to fix a problem in my design.
Home /Software Forums/ S32 Design Studio Knowledge Base/ HOWTO: Run a routine from RAM in S32 Design Studio
HOWTO: Run a routine from RAM in S32 Design Studio - NXP Community
The post mentions that the problem is fixed in the latest version of S32, but the problem still exists for me.
S32 Design Studio for Power Architecture
Version 2017.R1
Build Id 171018
Thanks for your help,
Hi,
Thanks for your reply.
I am sorry for the late reply. I was out sick.
The compiler is not being updated to the February version you posted.
I updated to version 3.
S32 Design Studio for Power Architecture 2017.R1 Update 3 - S32Rx7x SDK EAR 0.8.3
I am still getting the Error and the gcc version remains the same.
I tried updating to
S32 Design Studio for Power Architecture 2017.R1 Update 3 - S32Rx7x SDK EAR 0.8.3
Which should be the update I need, but I did not see the compiler update.
This version mentions the gcc version 4.9.4 update, but it is a Tar ball, which I am not familiar with, so I opted for the Zip version
Compiler and Build Tools Source Package – GCC v4.9.4 for S32 Design Studio for Power Architecture® 2017.R1 Update 2(REV UP2)
Thank you,
I finally ended up giving up on trying to fix S32 Version 2017.R1 and updated to S32 Version 2.1.
I have been putting off updating S32, but this issue needed fixing.
I had to fix a few issues with the paths not pointing to the correct tools. Nothing is ever easy.
As far as S32 2017.R1, no matter what I tried upgrading to, I still got the same powerpc-eabivle-gcc version.
In conclusion, it works now.
Thank you,