How to reverse bitfield arrangement?
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi,
I have a structure that contains bitfields in code. The question is on how to change the arrangement order of the bitfields within the byte.
Instead of having it arranged from MSB to LSB, (What S32 DS doing by default)
typedef struct
{
uint8_t a:4;
uint8_t b:3;
} test;
LSB 0 1 2 3 4 5 6 7 MSB
none b0 b1 b2 a0 a1 a2 a3
I would like to make it arranged from LSB to MSB,
typedef struct
{
uint8_t a:4;
uint8_t b:3;
} test;
LSB 0 1 2 3 4 5 6 7 MSB
a0 a1 a2 a3 b0 b1 b2 none
This issue caused very serious problems on CAN communication legacy code as all the signals are defined as bitfields.
In CodeWarrior, there was an option to config the compiler:
#pragma reverse_bitfields on
http://www.nxp.com/docs/en/reference-manual/CCOMPILERRM.pdf Page 192
I would like how to do the same settings in S32 DS. Thanks in advance!
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Bitfiled allocation is not detined by standard and compiler do whatever he wants with this. Although most of compilers doesn't change fields order inside of.
The simpliest way to support bi-endian is to use follwoing wrapper:
#ifdef LITTLE_ENDIAN /* Little endian order */
#define BITFIELDS_02(a01, a02) \
a01; a02;
#elif defined BIG_ENDIAN
#define BITFIELDS_02(a01, a02) \
a02; a01;#else
#error "Endianess not defined"
#endif
typedef struct
{
BITFIELDS_02(
uint8_t a:4,
uint8_t b:3,
)
} test;
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hello,
I'm afraid that #pragma revese_bitfields on is no more supported by gcc version 4. There is similar question on stackoverflow site.
Best way how to solve your issue is rewrite your structure definitions or do bit swap when you receive message from CAN bus.
Jiri