How to download the code with S32DS for PA V1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to download the code with S32DS for PA V1.1

跳至解决方案
2,628 次查看
boshimao
Contributor II

Hi NXP
      I want to know how to download the code to flash ?

标签 (2)
标记 (2)
0 项奖励
回复
1 解答
2,291 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

I am afraid it is not possible to download code without starting debug session. So there is simple solution. Start debug session, download the code and kill the debug session.

Regards,
Martin

在原帖中查看解决方案

0 项奖励
回复
6 回复数
2,291 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

click Debug icon in the IDE and wait, until code is loaded into the microcontroller.

pastedImage_1.png

Regards,

Martin

0 项奖励
回复
2,291 次查看
boshimao
Contributor II

Hi,

Thank you for your answer, I can understand this, the Debug button can also download the code to the MCU FLASH and RAM, and the RUN button useless. If so, when I do not need to debug function is not too much trouble.

0 项奖励
回复
2,291 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

RUN button is not implemented in S32 Design Studio. If you need to configure debug settings, click debug configurations and choose the right ones, which are suitable for you. 

pastedImage_1.png

Regards,

Martin

0 项奖励
回复
2,291 次查看
boshimao
Contributor II

Hi

   My debug function is normal. I mean can download code only to flash.

0 项奖励
回复
2,292 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

I am afraid it is not possible to download code without starting debug session. So there is simple solution. Start debug session, download the code and kill the debug session.

Regards,
Martin

0 项奖励
回复
2,291 次查看
boshimao
Contributor II

Hi,

OK,thank you.

0 项奖励
回复