Building S32K146 project in S32DS from command line can't find library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Building S32K146 project in S32DS from command line can't find library

1,517 Views
tommy1231
Contributor II

I'm trying to build an S32K146 project in the S32DS 2.2 and it can't find a library

c:/nxp/s32ds_arm_v2.2/s32ds/build_tools/gcc_v6.3/gcc-6.3-arm32-eabi/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/real-ld.exe: cannot find -l:S32K14x_AMMCLIB.a

If I build the same project within the S32DS it builds correctly.

The library search path is set to

"${S32K14X_AMMCLIB_1.1.18_PATH}/lib/s32ds_arm32"

If I change this to point directly to it

C:\NXP\S32DS_ARM_v2.2\S32DS\software\AMMCLIB_v1.1.18\S32K14x_AMMCLIB_v1.1.18\lib\s32ds_arm32

Then it builds from the command line.

This is the command I'm using from the command line

eclipsec.exe -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data C:\Users\christom\workspaceS32DS.ARM.2.2_cmd -import C:\Users\christom\HED-MCU-Workspace\PM-04J-S32K -build PM_04J_S32K/App_Debug --launcher.suppressErrors

Looking for the best way to resolve

0 Kudos
Reply
2 Replies

1,451 Views
ErichStyger
Specialist I

It seems to me that it cannot resolve/find the variable S32K14X_AMMCLIB_1.1.18_PATH.

How did you define that variable? As CDT variable or in the workspace?

I did not try it, but maybe it works if you have that variable defined on console calling Eclipse?

0 Kudos
Reply

1,451 Views
tommy1231
Contributor II

I didn't define it, that was one of the default settings when S32DS created the project.  It can be found here in the linked resources

pastedImage_1.png

0 Kudos
Reply