Troubleshooting: Quick Fix Option in Problems View

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Troubleshooting: Quick Fix Option in Problems View

100% 有帮助 (1/1)

Troubleshooting: Quick Fix Option in Problems View

Quick Fix is a feature of the Java editor in Eclipse which enables a user to resolve problems found in the Java code of their project. This feature is available to be used within S32 Design Studio for some problems. Such problems will be identified with the 'light bulb' icon in the description field, as shown below:

pastedImage_2.png

For example, such problems sometimes occur when importing a project created in a previous version of S32 Design Studio, are provided from another user, or some files in a project have become corrupted.

To resolve issues identified with the 'light bulb' icon, right-click on the problem and from the pop-up menu, select 'Quick Fix'.

pastedImage_3.png

 The Quick Fix menu will appear, providing the available solutions for the problem. In most cases, there will be just one solution. Click finish to implement the fix.

pastedImage_4.png

In some cases, more information will be required from the user to complete the fix. Complete the form to provide the additional information, then click OK.

pastedImage_5.png

Now the problem should be resolved.

评论

Thanks for the sharing! The warning of the type "S32 project version problem" and "The hardware settings required for project" can be fixed by referring to this article.

版本历史
最后更新:
‎11-08-2019 10:28 AM
更新人: