HOWTO: Generate S-Record/Intel HEX/Binary file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HOWTO: Generate S-Record/Intel HEX/Binary file

HOWTO: Generate S-Record/Intel HEX/Binary file

Right click on the Project name in Project Explorer -> Settings -> Cross Settings

pastedImage_1.png

Be sure to click Apply so the 'Standard S32DS Create Flash Image' section will appear In the Tool Settings tab.

pastedImage_2.png

Select 'General' under 'Standard S32DS Create Flash Image', now you can specify output in newly appeared option Standard S32DS Create flash image

pastedImage_2.png

标签 (1)
评论

Hello,

I followed your steps. To create the binary file for the bootloader using position indepenedent code. But my application is generating .srec file. Which I believe will not work with bootloader. So I tried to create .bin file using the raw binary option. And I tried to flash this file using bootloader. But it is not able to boot the application code after flashing the bin file to the S32K144 evb. Please help

Thank you

无评分
版本历史
最后更新:
‎07-04-2018 11:33 PM
更新人: