what is the procedure to handle unused port pins of part MC9S12XET256MAG ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the procedure to handle unused port pins of part MC9S12XET256MAG ?

592件の閲覧回数
kumara
Contributor I
0 件の賞賛
返信
2 返答(返信)

431件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

The http://www.nxp.com/docs/en/application-note/AN3262.pdf written for S12XD family devices can be used to better understand design. Of course, there are some differences between devices but the HW design is almost the same and technical approach is common.

The Chapter 14 describes Managing Unused Pins.

Best regards,

Ladislav

0 件の賞賛
返信

431件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Unused pins can be configured as inputs or outputs. But because internal pull resistors are active only in the input mode, it is better to set them as inputs and enable pullups. Many pins have pullups enabled by default, out of reset.

 

Regards,

Daniel

0 件の賞賛
返信