Missed TIMER input capture edge interrupt mc9s12xs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Missed TIMER input capture edge interrupt mc9s12xs

852 次查看
Florijan
Contributor III

Hello,

 

i have an application in which i have to count 3000 pulses of 120khz input square signal. I am using input capture on timer module to trigger interrupt on positive edge of 120khz input signal. Sometimes one interrupt is not generated and one pulse is not counted. So 3000 pulses lasts for 3001 pulse long. this happens rarely (once per 20s) but it happens. Does anyone have any idea why this is happening. In my application it is critical that interrupts are not missed. The mcu is working on 32Mhz bus clock. Can anyone say what should be the slew rate of measured square signal? Right now it is 50 ns. I am convinced that the there is a hardware problem inside mcu.

 

Best regards,

Florijan

标签 (1)
0 项奖励
5 回复数

600 次查看
kef2
Senior Contributor IV

Rise time of 50ns is OK. The more important is minimum pulse width, which must be longer than ECLK period.

Aren't you are late servicing all interrupts in time? For robust ISR handling the sum of all your ISR execution times should be less then 1/120kHz. 32M / 120k = 266 bus cycles - not a lot.

Are you using several timer channel interrupts? If so, then this thread applies to you to

Why clearing RTIF bit will cause PORF, LVRF bit cleared also for S12 MCU?

0 项奖励

600 次查看
Florijan
Contributor III

Hi Edward,

Thank you for fast reply.

I am using only one interrupt (mentioned). The pulse duty cycle is around 50%. I am using only one timer channel so clearing channel flag is not an issue.

The init code is:

void MCU_init(void)

{

  /* ### MC9S12XS256_112 "Cpu" init code ... */

  /*  PE initialization code after reset */

  /*  System clock initialization */

  /* CLKSEL: PLLSEL=0,PSTP=0,XCLKS=0,PLLWAI=0,RTIWAI=0,COPWAI=0 */

  CLKSEL = 0x00U;                      /* Select clock source from XTAL and set bits in CLKSEL reg. */

  /* PLLCTL: CME=1,PLLON=0,FM1=0,FM0=0,FSTWKP=0,PRE=0,PCE=0,SCME=0 */

  PLLCTL = 0x80U;                      /* Disable the PLL */

  /* SYNR: VCOFRQ1=0,VCOFRQ0=1,SYNDIV5=0,SYNDIV4=0,SYNDIV3=0,SYNDIV2=1,SYNDIV1=1,SYNDIV0=1 */

  SYNR = 0x47U;                        /* Set the multiplier register */

  /* REFDV: REFFRQ1=0,REFFRQ0=1,REFDIV5=0,REFDIV4=0,REFDIV3=0,REFDIV2=0,REFDIV1=0,REFDIV0=0 */

  REFDV = 0x40U;                       /* Set the divider register */

  /* POSTDIV: POSTDIV4=0,POSTDIV3=0,POSTDIV2=0,POSTDIV1=0,POSTDIV0=0 */

  POSTDIV = 0x00U;                     /* Set the post divider register */

  /* PLLCTL: CME=1,PLLON=1,FM1=0,FM0=0,FSTWKP=0,PRE=0,PCE=0,SCME=0 */

  PLLCTL = 0xC0U;                                     

  while(CRGFLG_LOCK == 0U) {           /* Wait until the PLL is within the desired tolerance of the target frequency */

  }

  /* CLKSEL: PLLSEL=1 */

  CLKSEL |= (unsigned char)0x80U;      /* Select clock source from PLL */

  /* VREGHTCL: VSEL=0,VAE=1,HTEN=0,HTDS=0,HTIE=0,HTIF=0 */

  VREGHTCL = 0x10U;                                     

  /* Int. priority initialization */

  /*                                        No. Address Pri XGATE Name           Description */

  INT_CFADDR = 0x10U;                                     

  INT_CFDATA2 = 0x01U;                 /*  0x0A  0xFF14   1   no   ivVReserved118 unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x0B  0xFF16   1   no   ivVReserved117 unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x0C  0xFF18   1   no   ivVReserved116 unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x0D  0xFF1A   1   no   ivVReserved115 unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x0E  0xFF1C   1   no   ivVReserved114 unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x0F  0xFF1E   1   no   ivVReserved113 unused by PE */

  INT_CFADDR = 0x20U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x10  0xFF20   1   no   ivVReserved112 unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x11  0xFF22   1   no   ivVReserved111 unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x12  0xFF24   1   no   ivVReserved110 unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x13  0xFF26   1   no   ivVReserved109 unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x14  0xFF28   1   no   ivVReserved108 unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x15  0xFF2A   1   no   ivVReserved107 unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x16  0xFF2C   1   no   ivVReserved106 unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x17  0xFF2E   1   no   ivVReserved105 unused by PE */

  INT_CFADDR = 0x30U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x18  0xFF30   1   no   ivVReserved104 unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x19  0xFF32   1   no   ivVReserved103 unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x1A  0xFF34   1   no   ivVReserved102 unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x1B  0xFF36   1   no   ivVReserved101 unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x1C  0xFF38   1   no   ivVReserved100 unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x1D  0xFF3A   1   no   ivVReserved99  unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x1E  0xFF3C   1   no   ivVReserved98  unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x1F  0xFF3E   1   no   ivVatd0compare unused by PE */

  INT_CFADDR = 0x40U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x20  0xFF40   1   no   ivVReserved96  unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x21  0xFF42   1   no   ivVReserved95  unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x22  0xFF44   1   no   ivVReserved94  unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x23  0xFF46   1   no   ivVReserved93  unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x24  0xFF48   1   no   ivVReserved92  unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x25  0xFF4A   1   no   ivVReserved91  unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x26  0xFF4C   1   no   ivVReserved90  unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x27  0xFF4E   1   no   ivVReserved89  unused by PE */

  INT_CFADDR = 0x50U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x28  0xFF50   1   no   ivVReserved88  unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x29  0xFF52   1   no   ivVReserved87  unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x2A  0xFF54   1   no   ivVReserved86  unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x2B  0xFF56   1   no   ivVReserved85  unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x2C  0xFF58   1   no   ivVReserved84  unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x2D  0xFF5A   1   no   ivVReserved83  unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x2E  0xFF5C   1   no   ivVReserved82  unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x2F  0xFF5E   1   no   ivVReserved81  unused by PE */

  INT_CFADDR = 0x60U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x30  0xFF60   1   no   ivVReserved79  unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x31  0xFF62   1   no   ivVReserved78  unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x32  0xFF64   1   no   ivVReserved77  unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x33  0xFF66   1   no   ivVReserved76  unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x34  0xFF68   1   no   ivVReserved75  unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x35  0xFF6A   1   no   ivVReserved74  unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x36  0xFF6C   1   no   ivVReserved73  unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x37  0xFF6E   1   no   ivVReserved72  unused by PE */

  INT_CFADDR = 0x70U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x38  0xFF70   1   no   ivVReserved71  unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x39  0xFF72   1   no   ivVReserved70  unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x3A  0xFF74   1   no   ivVpit3        unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x3B  0xFF76   1   no   ivVpit2        unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x3C  0xFF78   1   no   ivVpit1        unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x3D  0xFF7A   1   no   ivVpit0        unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x3E  0xFF7C   1   -    ivVhti         unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x3F  0xFF7E   1   no   ivVapi         unused by PE */

  INT_CFADDR = 0x80U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x40  0xFF80   1   no   ivVlvi         unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x41  0xFF82   1   no   ivVReserved62  unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x42  0xFF84   1   no   ivVReserved61  unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x43  0xFF86   1   no   ivVReserved60  unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x44  0xFF88   1   no   ivVReserved59  unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x45  0xFF8A   1   no   ivVReserved58  unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x46  0xFF8C   1   no   ivVpwmesdn     used by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x47  0xFF8E   1   no   ivVportp       used by PE */

  INT_CFADDR = 0x90U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x48  0xFF90   1   no   ivVReserved55  unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x49  0xFF92   1   no   ivVReserved54  unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x4A  0xFF94   1   no   ivVReserved53  unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x4B  0xFF96   1   no   ivVReserved52  unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x4C  0xFF98   1   no   ivVReserved51  unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x4D  0xFF9A   1   no   ivVReserved50  unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x4E  0xFF9C   1   no   ivVReserved49  unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x4F  0xFF9E   1   no   ivVReserved48  unused by PE */

  INT_CFADDR = 0xA0U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x50  0xFFA0   1   no   ivVReserved47  unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x51  0xFFA2   1   no   ivVReserved46  unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x52  0xFFA4   1   no   ivVReserved45  unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x53  0xFFA6   1   no   ivVReserved44  unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x54  0xFFA8   1   no   ivVReserved43  unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x55  0xFFAA   1   no   ivVReserved42  unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x56  0xFFAC   1   no   ivVReserved41  unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x57  0xFFAE   1   no   ivVReserved40  unused by PE */

  INT_CFADDR = 0xB0U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x58  0xFFB0   1   no   ivVcan0tx      unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x59  0xFFB2   1   no   ivVcan0rx      unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x5A  0xFFB4   1   no   ivVcan0err     unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x5B  0xFFB6   1   no   ivVcan0wkup    unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x5C  0xFFB8   1   no   ivVflash       used by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x5D  0xFFBA   1   no   ivVflashfd     used by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x5E  0xFFBC   1   no   ivVReserved33  unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x5F  0xFFBE   1   no   ivVReserved32  unused by PE */

  INT_CFADDR = 0xC0U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x60  0xFFC0   1   no   ivVReserved31  unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x61  0xFFC2   1   no   ivVReserved30  unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x62  0xFFC4   1   no   ivVcrgscm      unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x63  0xFFC6   1   no   ivVcrgplllck   unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x64  0xFFC8   1   no   ivVReserved27  unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x65  0xFFCA   1   no   ivVReserved26  unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x66  0xFFCC   1   no   ivVporth       unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x67  0xFFCE   1   no   ivVportj       unused by PE */

  INT_CFADDR = 0xD0U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x68  0xFFD0   1   no   ivVReserved23  unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x69  0xFFD2   1   no   ivVatd0        unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x6A  0xFFD4   1   no   ivVsci1        unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x6B  0xFFD6   1   no   ivVsci0        unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x6C  0xFFD8   1   no   ivVspi0        unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x6D  0xFFDA   1   no   ivVtimpaie     used by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x6E  0xFFDC   1   no   ivVtimpaaovf   used by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x6F  0xFFDE   1   no   ivVtimovf      used by PE */

  INT_CFADDR = 0xE0U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x70  0xFFE0   1   no   ivVtimch7      unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x71  0xFFE2   1   no   ivVtimch6      unused by PE */

  INT_CFDATA2 = 0x01U;                 /*  0x72  0xFFE4   1   no   ivVtimch5      unused by PE */

  INT_CFDATA3 = 0x01U;                 /*  0x73  0xFFE6   1   no   ivVtimch4      unused by PE */

  INT_CFDATA4 = 0x01U;                 /*  0x74  0xFFE8   1   no   ivVtimch3      unused by PE */

  INT_CFDATA5 = 0x01U;                 /*  0x75  0xFFEA   1   no   ivVtimch2      unused by PE */

  INT_CFDATA6 = 0x01U;                 /*  0x76  0xFFEC   1   no   ivVtimch1      unused by PE */

  INT_CFDATA7 = 0x01U;                 /*  0x77  0xFFEE   1   no   ivVtimch0      used by PE */

  INT_CFADDR = 0xF0U;                                     

  INT_CFDATA0 = 0x01U;                 /*  0x78  0xFFF0   1   no   ivVrti         unused by PE */

  INT_CFDATA1 = 0x01U;                 /*  0x79  0xFFF2   1   no   ivVirq         unused by PE */

  /* Common initialization of the CPU registers */

  /* RDRP: RDRP7=0,RDRP6=0,RDRP5=1,RDRP4=0,RDRP3=0,RDRP2=0,RDRP1=0,RDRP0=1 */

  RDRP = 0x21U;                                     

  /* PTTRR: PTTRR5=0 */

  PTTRR &= (unsigned char)~(unsigned char)0x20U;                    

  /* PPSP: PPSP0=0 */

  PPSP &= (unsigned char)~(unsigned char)0x01U;                    

  /* PERP: PERP0=1 */

  PERP |= (unsigned char)0x01U;                     

  /* COPCTL: WCOP=0,RSBCK=1,CR2=0,CR1=1,CR0=1 */

  COPCTL = (COPCTL & (unsigned char)~(unsigned char)0x84U) | (unsigned char)0x43U;

  /* CRGINT: LOCKIE=0,SCMIE=0 */

  CRGINT &= (unsigned char)~(unsigned char)0x12U;                    

  /* VREGCTRL: LVIE=0 */

  VREGCTRL &= (unsigned char)~(unsigned char)0x02U;                    

  /* RDRIV: RDPK=0,RDPE=0,RDPB=0,RDPA=0 */

  RDRIV &= (unsigned char)~(unsigned char)0x93U;                    

  /* RDRH: RDRH7=0,RDRH6=0,RDRH5=0,RDRH4=0,RDRH3=0,RDRH2=0,RDRH1=0,RDRH0=0 */

  RDRH = 0x00U;                                     

  /* RDRJ: RDRJ7=0,RDRJ6=0,RDRJ1=0,RDRJ0=0 */

  RDRJ &= (unsigned char)~(unsigned char)0xC3U;                    

  /* RDRM: RDRM7=0,RDRM6=0,RDRM5=0,RDRM4=0,RDRM3=0,RDRM2=0,RDRM1=0,RDRM0=0 */

  RDRM = 0x00U;                                     

  /* RDRS: RDRS7=0,RDRS6=0,RDRS5=0,RDRS4=0,RDRS3=0,RDRS2=0,RDRS1=0,RDRS0=0 */

  RDRS = 0x00U;                                     

  /* RDRT: RDRT7=0,RDRT6=0,RDRT5=1,RDRT4=0,RDRT3=0,RDRT2=0,RDRT1=0,RDRT0=0 */

  RDRT = 0x20U;                                     

  /* RDR0AD0: RDR0AD07=0,RDR0AD06=0,RDR0AD05=0,RDR0AD04=0,RDR0AD03=0,RDR0AD02=0,RDR0AD01=0,RDR0AD00=0 */

  RDR0AD0 = 0x00U;                                     

  /* RDR1AD0: RDR1AD07=0,RDR1AD06=0,RDR1AD05=0,RDR1AD04=0,RDR1AD03=0,RDR1AD02=0,RDR1AD01=0,RDR1AD00=0 */

  RDR1AD0 = 0x00U;                                     

  /* IRQCR: IRQEN=0 */

  IRQCR &= (unsigned char)~(unsigned char)0x40U;                    

  /* ### Init_PWM init code */

  /* PWME: PWME7=0,PWME6=0,PWME5=0,PWME4=0,PWME3=0,PWME2=0,PWME1=0,PWME0=0 */

  PWME = 0x00U;                        /* Disable all PWM channels */

  /* PWMPOL: PPOL7=0,PPOL6=0,PPOL5=1,PPOL4=0,PPOL3=0,PPOL2=0,PPOL1=1,PPOL0=0 */

  PWMPOL = 0x22U;                                     

  /* PWMCLK: PCLK7=0,PCLK6=0,PCLK5=0,PCLK4=0,PCLK3=0,PCLK2=0,PCLK1=1,PCLK0=0 */

  PWMCLK = 0x02U;                                     

  /* PWMCAE: CAE7=0,CAE6=0,CAE5=0,CAE4=0,CAE3=0,CAE2=0,CAE1=0,CAE0=0 */

  PWMCAE = 0x00U;                                     

  /* PWMCTL: CON67=0,CON45=1,CON23=0,CON01=1,PSWAI=1,PFRZ=0 */

  PWMCTL = 0x58U;                                     

  /* PWMDTY01: PWMDTY01=0 */

  PWMDTY01 = 0x00U;                           

  /* PWMPER01: PWMPER01=0xFFFF */

  PWMPER01 = 0xFFFFU;                           

  /* PWMDTY45: PWMDTY45=0x8000 */

  PWMDTY45 = 0x8000U;                           

  /* PWMPER45: PWMPER45=0xFFFF */

  PWMPER45 = 0xFFFFU;                           

  /* PWMSCLA: BIT7=0,BIT6=0,BIT5=0,BIT4=1,BIT3=0,BIT2=0,BIT1=0,BIT0=0 */

  PWMSCLA = 0x10U;                                     

  /* PWMSCLB: BIT7=0,BIT6=0,BIT5=0,BIT4=0,BIT3=0,BIT2=1,BIT1=1,BIT0=0 */

  PWMSCLB = 0x06U;                                     

  /* PWMPRCLK: PCKB2=0,PCKB1=0,PCKB0=0,PCKA2=0,PCKA1=0,PCKA0=0 */

  PWMPRCLK = 0x00U;                                     

  /* PWMSDN: PWMIF=1,PWMIE=0,PWMRSTRT=1,PWMLVL=0,PWM7IN=0,PWM7INL=0,PWM7ENA=0 */

  PWMSDN = 0xA0U;                                     

  /* PWME: PWME7=0,PWME6=0,PWME5=1,PWME4=0,PWME3=0,PWME2=0,PWME1=1,PWME0=0 */

  PWME = 0x22U;                        /* Enable only configured PWM channels */

  /* ### Init_TIM init code */

  /* TSCR1: TEN=0 */

  TSCR1 &= (unsigned char)~(unsigned char)0x80U;                    

  /* TIE: C7I=0,C6I=0,C5I=0,C4I=0,C3I=0,C2I=0,C1I=0,C0I=0 */

  TIE = 0x00U;                                     

  /* PACTL: PAEN=0,PAI=0 */

  PACTL &= (unsigned char)~(unsigned char)0x41U;                    

  /* PTTRR: PTTRR7=0,PTTRR6=0,PTTRR5=0,PTTRR4=0,PTTRR2=0,PTTRR1=0,PTTRR0=1 */

  PTTRR = 0x01U;                                     

  /* TIOS: IOS7=0,IOS6=0,IOS5=0,IOS4=0,IOS3=0,IOS2=0,IOS1=0,IOS0=0 */

  TIOS = 0x00U;                                     

  /* TC0: BIT15=0,BIT14=0,BIT13=0,BIT12=0,BIT11=0,BIT10=0,BIT9=0,BIT8=0,BIT7=0,BIT6=0,BIT5=0,BIT4=0,BIT3=0,BIT2=0,BIT1=0,BIT0=0 */

  TC0 = 0x00U;                           

  /* OCPD: OCPD7=0,OCPD6=0,OCPD5=0,OCPD4=0,OCPD3=0,OCPD2=0,OCPD1=0,OCPD0=1 */

  OCPD = 0x01U;                                     

  /* OC7M: OC7M7=0,OC7M6=0,OC7M5=0,OC7M4=0,OC7M3=0,OC7M2=0,OC7M1=0,OC7M0=0 */

  OC7M = 0x00U;                                     

  /* OC7D: OC7D7=0,OC7D6=0,OC7D5=0,OC7D4=0,OC7D3=0,OC7D2=0,OC7D1=0,OC7D0=0 */

  OC7D = 0x00U;                                     

  /* TTOV: TOV7=0,TOV6=0,TOV5=0,TOV4=0,TOV3=0,TOV2=0,TOV1=0,TOV0=0 */

  TTOV = 0x00U;                                     

  /* TCTL1: OM7=0,OL7=0,OM6=0,OL6=0,OM5=0,OL5=0,OM4=0,OL4=0 */

  TCTL1 = 0x00U;                                     

  /* TCTL2: OM3=0,OL3=0,OM2=0,OL2=0,OM1=0,OL1=0,OM0=0,OL0=0 */

  TCTL2 = 0x00U;                                     

  /* TCTL3: EDG7B=0,EDG7A=0,EDG6B=0,EDG6A=0,EDG5B=0,EDG5A=0,EDG4B=0,EDG4A=0 */

  TCTL3 = 0x00U;                                     

  /* TCTL4: EDG3B=0,EDG3A=0,EDG2B=0,EDG2A=0,EDG1B=0,EDG1A=0,EDG0B=0,EDG0A=1 */

  TCTL4 = 0x01U;                                     

  /* TFLG1: C7F=1,C6F=1,C5F=1,C4F=1,C3F=1,C2F=1,C1F=1,C0F=1 */

  TFLG1 = 0xFFU;                                     

  /* TFLG2: TOF=1 */

  TFLG2 = 0x80U;                                     

  /* TIE: C7I=0,C6I=0,C5I=0,C4I=0,C3I=0,C2I=0,C1I=0,C0I=1 */

  TIE = 0x01U;                                     

  /* TSCR2: TOI=0,TCRE=0,PR2=0,PR1=0,PR0=0 */

  TSCR2 = 0x00U;                                     

  /* PACNT: BIT15=0,BIT14=0,BIT13=0,BIT12=0,BIT11=0,BIT10=0,BIT9=0,BIT8=0,BIT7=0,BIT6=0,BIT5=0,BIT4=0,BIT3=0,BIT2=0,BIT1=0,BIT0=0 */

  PACNT = 0x00U;                           

  /* PTPSR: PTPS7=0,PTPS6=0,PTPS5=0,PTPS4=0,PTPS3=0,PTPS2=0,PTPS1=0,PTPS0=0 */

  PTPSR = 0x00U;                                     

  /* TSCR1: TEN=1,TSWAI=1,TSFRZ=1,TFFCA=1,PRNT=0 */

  TSCR1 = 0xF0U;                                     

  /* PAFLG: PAOVF=1,PAIF=1 */

  PAFLG = 0x03U;                                     

  /* PACTL: PAEN=0,PAMOD=0,PEDGE=0,CLK1=0,CLK0=0,PAOVI=0,PAI=0 */

  PACTL = 0x00U;                                     

  /* ### Init_FLASH init code */

  /* FERSTAT: DFDIF=1,SFDIF=1 */

  FERSTAT = 0x03U;                                     

  /* FSTAT: CCIF=0,ACCERR=1,FPVIOL=1,MGBUSY=0,MGSTAT1=0,MGSTAT0=0 */

  FSTAT = 0x30U;                       /* Clear error flags ACCERR and FPVIOL */

  /* FPROT: FPOPEN=1,RNV6=1,FPHDIS=1,FPHS1=1,FPHS0=1,FPLDIS=1,FPLS1=1,FPLS0=1 */

  FPROT = 0xFFU;                                     

  /* DFPROT: DPOPEN=1,DPS4=0,DPS3=0,DPS2=0,DPS1=0,DPS0=0 */

  DFPROT = 0x80U;                                     

  /* FERCNFG: DFDIE=0,SFDIE=0 */

  FERCNFG = 0x00U;                                     

  /* FCNFG: CCIE=0,IGNSF=0,FDFD=0,FSFD=0 */

  FCNFG = 0x00U;                                     

  /* FCLKDIV: FDIVLD=0,FDIV6=0,FDIV5=0,FDIV4=0,FDIV3=0,FDIV2=1,FDIV1=0,FDIV0=0 */

  FCLKDIV = 0x04U;                                     

  /* ### Init_COP init code */

  /* CLKSEL: COPWAI=1 */

  CLKSEL |= (unsigned char)0x01U;                     

  /* PLLCTL: PCE=1 */

  PLLCTL |= (unsigned char)0x02U;                     

  /* ### Init_GPIO init code */

    /* Disable interrupts */

  /* PIEP: PIEP7=0,PIEP6=0,PIEP5=0,PIEP4=0,PIEP3=0,PIEP2=0,PIEP1=0,PIEP0=0 */

  PIEP = 0x00U;                                     

    /* Clear interrupt flags */

  /* PIFP: PIFP7=1,PIFP6=1,PIFP5=1,PIFP4=1,PIFP3=1,PIFP2=1,PIFP1=1,PIFP0=1 */

  PIFP = 0xFFU;                                     

  /* DDRP: DDRP3=1 */

  DDRP |= (unsigned char)0x08U;                     

  /* ### Init_GPIO init code */

  /* PORTA: PA0=0 */

  PORTA &= (unsigned char)~(unsigned char)0x01U;                    

  /* DDRA: DDRA0=1 */

  DDRA |= (unsigned char)0x01U;                     

  /* ### */

  /* Initial interrupt priority */

  /*lint -save  -e950 Disable MISRA rule (1.1) checking. */

  asm CLI;                             /* Enable interrupts */

  /*lint -restore Enable MISRA rule (1.1) checking. */

} /*MCU_init*/

The ISR code is:

unsigned char   measurementCH0_finished=0;

unsigned int NumberOfPulsesToCountCH0=3000;

unsigned int ValueCH0atStart;

unsigned int ValueCH0End;

unsigned int ValueCH0Temp;

unsigned int NumberOfOverflowsCH0;

unsigned char  FirstTimeCH0;

unsigned int TC0_temp;

void InterruptCH0(void){

               TFLG1_C0F=1; //flag

          //      PORTA_PA0=1;

               TC0_temp= TC0;

               if(FirstTimeCH0) {

                    ValueCH0atStart=TC0_temp;

                    ValueCH0Temp=ValueCH0atStart;

                     FirstTimeCH0=0;

               } else{

                     if(ValueCH0Temp>TC0_temp){

                             NumberOfOverflowsCH0+=1;

                     }

                    ValueCH0Temp= TC0_temp;

               }

               if(NumberOfPulsesToCountCH0==0){

                         ValueCH0End=TC0_temp;

                          TIE_C0I=0; // interrupt

                        //  PORTA_PA0=0;

                          measurementCH0_finished=1;

               } else{

                    NumberOfPulsesToCountCH0-=1;

               }             

                

}

Best regards,

Florijan

0 项奖励

600 次查看
kef2
Senior Contributor IV

With TFFC==1, sequence to clear timer flags is different. Writes to TFLG1 are ignored. For input capture channel you need to read TCx to clear timer flag. Try replacing your TFFC1 = 0xFF; with read from TC0 and check if it helps.

600 次查看
Florijan
Contributor III

Finally I found the solution. I forgot to clear TFLG1_C0F interrupt flag before a whole measurement. Now everything works ok.

Thank you Edward for useful comments.

Best regards,

Floriijan

0 项奖励

600 次查看
Florijan
Contributor III

I do have read from TC0 already.

The ISR code is:

unsigned char   measurementCH0_finished=0;

unsigned int NumberOfPulsesToCountCH0=3000;

unsigned int ValueCH0atStart;

unsigned int ValueCH0End;

unsigned int ValueCH0Temp;

unsigned int NumberOfOverflowsCH0;

unsigned char  FirstTimeCH0;

unsigned int TC0_temp;

void InterruptCH0(void){

               TFLG1_C0F=1; //flag

          //      PORTA_PA0=1;

               TC0_temp= TC0;    <---------------------------------------------------------------

               if(FirstTimeCH0) {

                    ValueCH0atStart=TC0_temp;

                    ValueCH0Temp=ValueCH0atStart;

                     FirstTimeCH0=0;

               } else{

                     if(ValueCH0Temp>TC0_temp){

                             NumberOfOverflowsCH0+=1;

                     }

                    ValueCH0Temp= TC0_temp;

               }

               if(NumberOfPulsesToCountCH0==0){

                         ValueCH0End=TC0_temp;

                          TIE_C0I=0; // interrupt

                        //  PORTA_PA0=0;

                          measurementCH0_finished=1;

               } else{

                    NumberOfPulsesToCountCH0-=1;

               }            

               

}

Best regards,

Florijan

0 项奖励