Flexray - SK-S12XDP512-A and (FRDC) FLXRAYIPMFR4200

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexray - SK-S12XDP512-A and (FRDC) FLXRAYIPMFR4200

3,049 Views
admin
Specialist II
Hi everyone
we are newbie with flexray and we are trying to develop a simple application with two nodes.
We bought two SK-S12XDP512-A evaluation board and two FLXRAYIPMFR4200 Generic Daughter Card.
We ask you: is the demo project included in the kit only for MFR4300?
Is there an application example that could run with MFR4200?
Thanks a lot for your attention
Paolo

Message Edited by Alban on 2006-12-22 10:07 AM

Labels (1)
0 Kudos
Reply
4 Replies

712 Views
NLFSJ
Contributor III
Hi,
 
I am not sure which demo project is included in the kit.
In case that it is FlexRay STARTER KIT (two SK-S12XDP512-A boards and two MFR4300 CC), the software CD should include the FlexRay UNIFIED Driver with application examples only for MFR4300.
 
If you have the SK-S12XDP512-A boards with different software CD, I'm not sure which FlexRay driver is provided.
 
However, the software status for Communication Controllers is as follows:
 
MFR4200 -
Freescale  provides the Low Level Driver (LLD) and/or High Level Driver (HLD). For both drivers, the application examples are created.
 
MFR4300 (and all new FlexRay modules) -
We provide the FlexRay UNIFIED Driver with application examples for required platforms.
 
Unfortunately, the LLD/HLD and the UNIFIED drivers are not compatible since there are too many changes in FlexRay module Controller Host Interface (CHI) concept.
 
I hope this helps.
 
Regards,
Nina
0 Kudos
Reply

712 Views
admin
Specialist II
Hi Nina,
thank you for your reply.
In the CD shipped with SK-S12XDP512-A there is the LLD and an application example for MFR4300 but I need the drivers for MFR4200.
Could you tell me how can I get them?
Could you explain me about the difference between LLD and HLD?
 
Best Regards
Paolo
 
 
0 Kudos
Reply

712 Views
vikram_iyengar
Contributor I
Paolo,

Try asking the Freescale to set up a compass Extranet where you get access to the LLDs and HLDs for different platforms.

You can use freescale's "service requests" link to reach them.

Let me know how it goes.

Cheers
Vi
0 Kudos
Reply

712 Views
admin
Specialist II
Hi
I've just got a Compass Extranet access, downloaded the HLDs and I'm fully operative.
 
Thank you very much.
Paolo
0 Kudos
Reply