speeding up DDR read in p4080

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

speeding up DDR read in p4080

287件の閲覧回数
nirlevy
Contributor I

HI,

I have noticed that the read operation from DDR ( i/o mem mapped) is 8 times slower than the write operations.

do you have any suggestions on how can I speed it up for blocks read?

The DDR id configured with SPD ( no ECC no interleaving)

0 件の賞賛
1 返信

232件の閲覧回数
Pavel
NXP Employee
NXP Employee

What is method is used for estimate read operations.

Look at the following documents for DDR setting:

https://www.nxp.com/docs/en/white-paper/CRSWP.pdf?fsrch=1&sr=1&pageNum=1

 

and

 

https://www.nxp.com/docs/en/supporting-information/WBNR_FTF10_NET_F0686.pdf?fsrch=1&sr=1&pageNum=3


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛