ls1043 usb 3.0 xhci

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1043 usb 3.0 xhci

100 Views
ggz
Contributor I

Hello *,

I attempted to configure the USB3.0 controller in "host" mode on the LS1043 platform. Based on observations, the XHCI controller initializes correctly;

however, when a USB device is connected, there is an abnormal increase in interrupt entries that prevents device recognition. Removing the device does not trigger any interrupts.

Can you assist me in analyzing this issue or suggest methods for analyzing interruptions from the XHCI interrupt controller?

Thank you.

0 Kudos
1 Reply

38 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "7.2.17.1 USB 3.0 Controller (DesignWare USB3)" in LSDKUG_Rev21.08.pdf.

0 Kudos