We are using LS1043A, IFC Chip select muxed with GPIO query

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We are using LS1043A, IFC Chip select muxed with GPIO query

457 Views
logeshs
Contributor II

we are connecting 3 devices with IFC of LS1043A which were NOR, and Two FPGA with CS0, CS1 and CS2. I wish to use CS3 as GPIO. Is there a Way? Where should i check in RCW? 

We are not using QSPI and Frequency Timer Module. If there is a way to use IFC_CS3 as GPIO please explain me how we shall make that setting.

0 Kudos
1 Reply

294 Views
alexander_yakov
NXP Employee
NXP Employee

No, all three pins IFC_CS_B[1:3] are configured by the same (only one) RCW field "IFC_GRP_E1_BASE"

Please look LS1043A Reference Manual, Table 3-9 for IFC pin multiplexing details.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos