Hello,
I know some pins for example CMOS inputs, open-drain outputs shouldn't be left floating except some special cases. Even If you are not using it.
There are some pins that I am not sure If I can leave them floating or not. I want to be sure that I can leave the following unused pins floating. Could anybody check please?
D1_MDM8
D1_MDQS8
D1_MDQS8_B
D1_MCS[1-3]_B
D1_MCKE[1-3]
D1_MCK[1-5]
D1_MCK[1-5]_B
The same pins of Memory Controller2
EVT[0-8]_B
SDHC_CLK
TSEC_1588_ALARM_OUT1
TSEC_1588_CLK_OUT
TSEC_1588_PULSE_OUT1
EMI1_MDC
EMI2_MDC
EMI2_MDIO
MDVAL
MSRCID0
MSRCID1
MSRCID2
Thank you
Sorry, EMI2_MDC and EMI2_MDIO pins shouldn't have been on the list above, my mistake. I already pulled these two pins to 1.2V
The board is highly intensive and I need to leave as more unused pins floating as possible. I don't uss ECC for the memory controllers of P4080 so can I leave D1_MECC[0-7] and D2_MECC[0-7] pins floating or should I tied them to GND?
Thanks in advance