Two Cooling fan P/N in the LS1046A RDB board where using?

取消
显示结果 
搜索替代 
您的意思是: 
已解决

Two Cooling fan P/N in the LS1046A RDB board where using?

跳至解决方案
927 次查看
michael_lee1
Contributor I

#LS1046A RDB,#BOM LS1046A,#ventilation fan P/N,cooling fan P/N

标记 (1)
0 项奖励
1 解答
628 次查看
ufedor
NXP Employee
NXP Employee

The provided data sheet is for the chassis fans.

在原帖中查看解决方案

7 回复数
628 次查看
michael_lee1
Contributor I

The RDB P/N is LS1046ARDB-PB.

Pls, check it over the document where the picture shown.

Ths,

0 项奖励
628 次查看
ufedor
NXP Employee
NXP Employee

Please see the fan data sheet attached.

0 项奖励
628 次查看
michael_lee1
Contributor I

Hi Ufedor,

 

Thanks a lot for the information.

Is it the same cooling fan using in the board where LS1046A processor cooling fan and other 2 side ventilation fans are same one, as provided P/N?

Thanks,

0 项奖励
629 次查看
ufedor
NXP Employee
NXP Employee

The provided data sheet is for the chassis fans.

628 次查看
michael_lee1
Contributor I

Thanks for the answer.

Can I have the information of the cooling fan P/N of the LS1046A in the top?

Pls, provided me the detail info and full P/N as well.

Regards,

0 项奖励
628 次查看
ufedor
NXP Employee
NXP Employee

There is no such fan on the LS1046ARDB-PB:

2019-01-21_160413.jpg

0 项奖励
628 次查看
ufedor
NXP Employee
NXP Employee

Which exactly RDB revision is in question?

Please provide a clear photo of the on-the-case stickers.

0 项奖励