TWR-LS1021A-PB with CPU1 not online

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-LS1021A-PB with CPU1 not online

1,375 Views
alessandromarin
Contributor I

Hello,

I'm using a TWR-LS1021A-PB development board.

The kernel version is:

 root@ls1021atwr:/proc# uname -a
Linux ls1021atwr 3.12.37-rt51+ls1+gf488de6 #2 SMP PREEMPT RT Tue Jun 21 13:37:12 CEST 2016 armv7l GNU/Linux

The board comes up with core0 only working.

I see the following message for core1:

CPU1: failed to come online

Can anyone give me suggestions?

thank you

0 Kudos
Reply
4 Replies

1,189 Views
ufedor
NXP Employee
NXP Employee

Please provide:

1) settings of all on-board switches

2) U-Boot log

0 Kudos
Reply

1,189 Views
alessandromarin
Contributor I

Hello,

The switch configuration is as follows:

SW3[1:8] OFF,ON,ON,OFF,OFF,ON,OFF,ON

SW2[1:8] OFF,OFF,ON,OFF,OFF,ON,OFF,ON

Thank you

0 Kudos
Reply

1,189 Views
ufedor
NXP Employee
NXP Employee

According to the U-Boot log the board has LS1021A Rev.1.0 and SDK v1.8 is the latest one supporting this silicon revision.

The SDK v1.9 and v2.0 support LS1021A Rev.2.0.

Do you see the same issue when precompiled image from SDK v1.8 is used and the board boots from NOR Flash?

0 Kudos
Reply

1,189 Views
alessandromarin
Contributor I

We have reconfigured the switches to boot from NOR Flash.

These are the messages from the board:

U-Boot 2014.01Layerscape-SDK-V1.3+g50d6848 (Oct 24 2014 - 19:21:22)

CPU: Freescale LayerScape LS1021E, Version: 1.0, (0x87081110)

Clock Configuration:

CPU0(ARMV7):1000 MHz,

Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

00000000: 0608000a 00000000 00000000 00000000

00000010: 70000000 00407900 e0025a00 21046000

00000020: 00000000 00000000 00000000 00038000

00000030: 00080000 48007340 00000000 00000000

Board: LS1021ATWR

CPLD: Vfb.fb

PCBA: Vfb.0

VBank: 1

I2C: ready

DRAM: 1 GiB (DDR3, 32-bit, CL=10.5, ECC off)

Using SERDES1 Protocol: 112 (0x70)

Flash: 128 MiB

MMC: FSL_SDHC: 0

      • Warning - bad CRC, using default environment

EEPROM: NXID v1

Firmware 'Microcode version 0.0.0 for T1040 r1.0' for 1040 V1.0

QE: uploading microcode 'Microcode for T1040 r1.0'

In: serial

Out: serial

Err: serial

SATA link 0 timeout.

AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode

flags: 64bit ncq pm clo only pmp fbss pio slum part ccc

scanning bus for devices...

Found 0 device(s).

Net: eTSEC2 is in sgmii mode.

eTSEC1 , eTSEC2, eTSEC3

=>

=>

Now how we have to proceed to have Linux working?

0 Kudos
Reply