T2081: Layout DDR3 and other High Speed Signals

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2081: Layout DDR3 and other High Speed Signals

Jump to solution
697 Views
ralftruebenbach
Contributor III

Hello,

our layout designer ask me if there are any information/data available about the chip internal length of the T2081 high speed signals. He would like to use this data to compensate the signal length in his design (or isn't that necessary?).

Kind regards,

Ralf

0 Kudos
1 Solution
570 Views
Bulat
NXP Employee
NXP Employee

It is not necessary, consider that all internal wires of each high speed interface are length matched. So the layout task should consider trace lengths between the T2081's pins and pins of external devices.

Regards,

Bulat

View solution in original post

0 Kudos
1 Reply
571 Views
Bulat
NXP Employee
NXP Employee

It is not necessary, consider that all internal wires of each high speed interface are length matched. So the layout task should consider trace lengths between the T2081's pins and pins of external devices.

Regards,

Bulat

0 Kudos