Hi,
We are going to use QorlQ T2080 Processor.
For Power calculation of the processor, Any excel/document is available to use?
Also, we are planning to use PCIe interface to NVMe SSD. As Processor will be root-complex and SSD will be End nodes, End nodes to be powered up and should be up before the root-complex, Should power sequence need to be taken care or processor will handle this??
And Processor will be End-point in another use case.
已解决! 转到解答。
Hi @KLN,
The required power sequencing is mentioned in the section# 3.2 of T2080 datasheet.
Regards,
Mrudang
Hi @mrudangshelat-13
I understand that Datasheet has mentioned power details in the datasheet.
I was specifically asking for the Excel is available for ease of use.
Also Please note that I have asked about SSD related question also.
Hi @KLN,
I apologize for the delay as I was facing some server glitches since last week.
I would suggest to implement a power switching circuit for the powering up the end node in order to avoid unwanted voltage to processor(root complex) from the end node when end node is powered up before the processor.
Regards,
Mrudang