Hi,
We are going to use QorlQ T2080 Processor.
For Power calculation of the processor, Any excel/document is available to use?
Also, we are planning to use PCIe interface to NVMe SSD. As Processor will be root-complex and SSD will be End nodes, End nodes to be powered up and should be up before the root-complex, Should power sequence need to be taken care or processor will handle this??
And Processor will be End-point in another use case.
解決済! 解決策の投稿を見る。
Hi @KLN,
The required power sequencing is mentioned in the section# 3.2 of T2080 datasheet.
Regards,
Mrudang
Hi @KLN,
Refer to section# 3.4 in the T12080 datasheet and specifically table# 8 for T2080 I/O power dissipation.
Regards,
Mrudang
Hi @mrudangshelat-13
I understand that Datasheet has mentioned power details in the datasheet.
I was specifically asking for the Excel is available for ease of use.
Also Please note that I have asked about SSD related question also.
Hi @KLN,
There is no such excel available.
Regarding the SSD related question, I am working on it and I will let you know once I have any findings.
Regards
Mrudang
Thanks for your response.
Please let us know at the earliest. I do see that responses are very slow.
Hi @KLN,
I apologize for the delay as I was facing some server glitches since last week.
I would suggest to implement a power switching circuit for the powering up the end node in order to avoid unwanted voltage to processor(root complex) from the end node when end node is powered up before the processor.
Regards,
Mrudang
Thanks for your response.
One more query on T2080 Evaluation board:
What is the purpose of connecting T2080's IFC to CPLD?
One more query on T2080 Power related,
Are there any requirement of Sequencing of power?
Hi @KLN,
The required power sequencing is mentioned in the section# 3.2 of T2080 datasheet.
Regards,
Mrudang