Please advise about EEE(Energy Efficient Ethernet) on LS1023A(/43A).

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Please advise about EEE(Energy Efficient Ethernet) on LS1023A(/43A).

1,294 次查看
kazuyayamauchi
Contributor II

Hi Experts,

We want to support IEEE802.3az (EEE: Energy Efficient Ethernet) on LS1023A(/43A).
From "6.2 mEMAC Features Summary" of LS1043ADPAARM(Rev.0), we understand that the LS1023A can support this.
However, we don't understand how to implement this feature with LS1023A.
Please advise which documents we should reference to.

Also, if any sample code, could you let us know?

Best Regards,

0 项奖励
3 回复数

1,036 次查看
norihiromichiga
Contributor V

Hello, 

ethtools with your suggested option allows us to enable eee, LPI.

>  ethtool --set-eee devname [eee on|off] [tx-lpi on|off] [tx-timer N] [advertise N]

LPI must be supported by hardware block in MAC layer on LS1043A.

Otherwise, above option is meaning less.

Can we think that above option can enable eee (sending LPI, detecting LPI) on MAC layer of LS1043A? 

Of course, we must use Ether PHY with 802.3az along with LS1043A.

Thanks,

Norihiro Michigami

AVNET 

0 项奖励

1,036 次查看
ufedor
NXP Employee
NXP Employee

There is no support for LPI on the LS1043.

0 项奖励

1,036 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the LSDK Documentation:

ethtool options 

0 项奖励