Hi,
I got LS1046ARDB and started booting it but the USB console port is not working. All the switches and jumpers are in default mode, but I realized that D8 LED is blinking when I plugged the USB console cable to PC with the board switched off. The D8 LED is off wheen I switch on the board, so I assume that the CMSIS-DAP firmware is not loaded.
Some months ago I worked with LS1043ARDB board and I had a similar problem that I solved following the steps that are in the next thread: LS1043ARDB-PD USB console can't work
However, in this case I could not found the *.bin file in the designer file.
Could somebody provide me the file that I should put in order to program the firmware?
Thanks in advance,
已解决! 转到解答。
As penman says in LS1012a RDB only appears as bootloader? , the firmware binary that is mentioned in the thread https://community.nxp.com/thread/483925 can be used for LS1046ARDB.
I have just tried and it works!
As penman says in LS1012a RDB only appears as bootloader? , the firmware binary that is mentioned in the thread https://community.nxp.com/thread/483925 can be used for LS1046ARDB.
I have just tried and it works!