LS1043A-RDB: LSDK 17.12: DDR4 timing: clocks vs nanoseconds

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A-RDB: LSDK 17.12: DDR4 timing: clocks vs nanoseconds

ソリューションへジャンプ
2,610件の閲覧回数
cyrilstrejc
Contributor III

I'm inspecting the LSDK 17.12 with the QorIQ LS1043A reference design board (LS1043A-RDB).

I'm confused by some of DDR4 timing settings:

In U-Boot, let's consider CONFIG_SYS_DDR_RAW_TIMING defined, the DDR4 timing is NOT read from the EEPROM, but it's hard-coded into the U-Boot's source code:

u-boot/board/freescale/ls1043ardb/ddr.c:

/* DDR model number: MT40A512M8HX-093E */
#ifdef CONFIG_SYS_DDR_RAW_TIMING
dimm_params_t ddr_raw_timing = {
     .n_ranks = 1,
     .rank_density = 2147483648u,
     .capacity = 2147483648u,
     .primary_sdram_width = 32,
     .ec_sdram_width = 0,
     .registered_dimm = 0,
     .mirrored_dimm = 0,
     .n_row_addr = 15,
     .n_col_addr = 10,
     .bank_addr_bits = 0,
     .bank_group_bits = 2,
     .edc_config = 0,
     .burst_lengths_bitmask = 0x0c,

     .tckmin_x_ps = 938,
     .tckmax_ps = 1500,
     .caslat_x = 0x000DFA00,
     .taa_ps = 13500,
     .trcd_ps = 13500,
     .trp_ps = 13500,
     .tras_ps = 33000,
     .trc_ps = 46500,
     .trfc1_ps = 260000,
     .trfc2_ps = 160000,
     .trfc4_ps = 110000,
     .tfaw_ps = 21000,
     .trrds_ps = 3700,
     .trrdl_ps = 5300,
     .tccdl_ps = 5355,
     .refresh_rate_ps = 7800000,

Let's focus for example to T_FAW. According to the Micron's datasheet, the minimum T_FAW for MT40A512M8-093E (DDR4-2133) should be "greater of 20CK of 21ns" (Table 157 of the datasheet). The MT40A512M8 page size is 1KB (Table 2 in the same datasheet).

micron-ddr4-tfaw.png

The tfaw_ps parameter of the structure is set correctly to 21ns (.tfaw_ps = 21000), but this leads to the TIMING_CFG_2 register of the LS1043A DDR registers is set to 0x0048C111, which means the FOUR_ACT in the register is set to 0x11 which means 17 cycles. I have read the TIMING_CFG_2 register value from U-Boot's prompt:

U-Boot 2017.07 (Jan 11 2018 - 10:01:08 +0100)

SoC: unknown (0x87920410)
Clock Configuration:
CPU0(A53):1600 MHz CPU1(A53):1600 MHz CPU2(A53):1600 MHz
CPU3(A53):1600 MHz
Bus: 400 MHz DDR: 1600 MT/s FMAN: 500 MHz
Reset Configuration Word (RCW):
00000000: 08100010 0a000000 00000000 00000000
00000010: 14550002 80004012 60040000 c1002000
00000020: 00000000 00000000 00000000 00038800
00000030: 00000000 00001100 00000096 00000001
...
Hit any key to stop autoboot: 0
=> md.l 108010C 1
0108010c: 11c14800

The number of cycles (17) respects 21ns minimum T_FAW time according to the datasheet, because 800MHz DDR clock means clock time 1.25ns and 17*1.25ns = 21.25ns, but it seems to me it does not respect statement in the datasheet, that minimum T_FAW should be "greater of 20CK or 21ns", the FOUR_ACT should be set to 20 cycles according to my understanding.

So, please, where is my understanding wrong? How it's possible the LSDK is happy with FOUR_ACT set to 17 cycles? 

0 件の賞賛
1 解決策
588件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please create a Technical Case referring the following:

https://community.nxp.com/thread/381898 

元の投稿で解決策を見る

0 件の賞賛
1 返信
589件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please create a Technical Case referring the following:

https://community.nxp.com/thread/381898 

0 件の賞賛