Is core-image will modify the default configuration and how to resolve it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is core-image will modify the default configuration and how to resolve it?

1,132 Views
yanggao
Contributor III

Hi,

I'm working with LS1043A and yocto poky, and I'm blocked by the following problem.

I add a new meta-layer in order to generate a custom image that integrates gdb and gdbserver. 

I have written my custom-image.bb is like follows in a new meta-custom directory:

---------------------------------------------------------------------------------------------------

SUMMARY = "A FIT image comprising the Linux image, dtb and rootfs"
LICENSE = "MIT"

KERNEL_IMAGETYPE := "Image"

KERNEL_IMAGE ?= "${KERNEL_IMAGETYPE}"
ROOTFS_IMAGE := "fsl-image-core"
KERNEL_ITS ?= "kernel.its"

SRC_URI = "file://${KERNEL_ITS}"

IMAGE_FEATURES +="dev-pkgs dbg-pkgs package-management tools-debug tools-sdk"
IMAGE_INSTALL += "\
    packagegroup-core-buildessential \
    packagegroup-core-tools-debug \
    packagegroup-core-tools-profile \
        "

inherit core-image custom-share-image

export IMAGE_BASENAME = "custom-image"

------------------------------------------------------------------------------------------------------------

And my custom-share-image.bbclass is like this:

---------------------------------------------------------------------------------------------------

PACKAGE_ARCH = "${MACHINE_ARCH}"

inherit deploy

do_patch[noexec] = "1"
do_configure[noexec] = "1"
do_compile[noexec] = "1"
do_install[noexec] = "1"
do_populate_sysroot[noexec] = "1"
do_package[noexec] = "1"
do_packagedata[noexec] = "1"
do_package_write_ipk[noexec] = "1"
do_package_write_deb[noexec] = "1"
do_package_write_rpm[noexec] = "1"

do_fetch[nostamp] = "1"
do_unpack[nostamp] = "1"
do_deploy[nostamp] = "1"
do_deploy[depends] += "virtual/kernel:do_build ${ROOTFS_IMAGE}:do_build"

do_deploy () {
    install -d ${DEPLOYDIR}
    cp ${DEPLOY_DIR_IMAGE}/${KERNEL_IMAGE} .
    rm -f ${KERNEL_IMAGE}.gz
    gzip ${KERNEL_IMAGE}
    for DTS_FILE in ${KERNEL_DEVICETREE}; do
        DTB_FILE="${KERNEL_IMAGETYPE}-`basename ${DTS_FILE}`";
        ITB_BASENAME=kernel-`basename ${DTS_FILE} |sed -e 's,.dtb$,,'`-${DATETIME}
        ITB_SYMLINk=kernel-`basename ${DTS_FILE} |sed -e 's,.dtb$,,'`

        cp ${WORKDIR}/${KERNEL_ITS} kernel.its
        sed -i -e "s,kernel-image.gz,${KERNEL_IMAGE}.gz," kernel.its
        sed -i -e "s,freescale.dtb,${DEPLOY_DIR_IMAGE}/${DTB_FILE}," kernel.its
        sed -i -e "s,rootfs.ext2.gz,${DEPLOY_DIR_IMAGE}/${ROOTFS_IMAGE}-${MACHINE}.ext2.gz," kernel.its

        mkimage -f kernel.its ${ITB_BASENAME}.itb

        install -m 644 ${ITB_BASENAME}.itb ${DEPLOYDIR}/
        ln -sf ${ITB_BASENAME}.itb ${DEPLOYDIR}/${ITB_SYMLINk}.itb
    done
}
addtask deploy before build

COMPATIBLE_MACHINE = "(fsl-lsch2|fsl-lsch3)"

-----------------------------------------------------------------------------------

When I run

$ bitbake custom-image

The deploy() of custom-share-image.bbclass is not executed and the kernel.itb is not generated. While, if I deleted "inherit core-image" in custom-image.bb file, deploy() is exectued but gdb and gdbserver are not integrated in rootfs. I think maybe some environment configurations are changed because core-image is inherited, but I can't locate it. Is there someone have the same problem like me? How do you resolve it? 

Thanks in advance! 

0 Kudos
1 Reply

862 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello yang gao,

Please add "packagegroup-core-tools-debug“  in the variable IMAGE_INSTALL_append of recipe meta-freescale/recipes-fsl/images/fsl-image-core.bb, please refer to the following, then rebuild itb image with the command "bitbake fsl-image-kernelitb".

IMAGE_INSTALL_append = " \
    packagegroup-fsl-tools-core \
    packagegroup-fsl-benchmark-core \
    packagegroup-fsl-networking-core \
    packagegroup-core-tools-debug \
"

Please refer to package list in poky/meta/recipes-core/packagegroups/packagegroup-core-tools-debug.bb.

RDEPENDS_${PN} = "\
    gdb \
    gdbserver \
    strace \
    ${MTRACE} \
    "


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos