In LS1043A, configuring the fpga using FPP x8 mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

In LS1043A, configuring the fpga using FPP x8 mode

807件の閲覧回数
logeshs
Contributor II

Hi,

We are using LS1043 and altera cyclone V fpga in our design. We like to configure the fpga using FPP x8 mode. Please refer the Cyclone V configuration datasheet

 

https://documentation.altera.com/#/00005773-AA$NT00072849

 

 

In our earlier design we have used NXP processors from MPC85xx series and we used the local bus to configure the altera fpga in FPP x8 mode. But in the LS1043 local bus (IFC bus) there is no UPM machine support (user programmable machine) . So how the programming can be implemented in the LS1043 system without glue logic.

Thanks

0 件の賞賛
返信
1 返信

670件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

I do not see possibility to use IFC instead of LBC in the very flexible UPM mode for the FPP 8x. From my point of view using the GPIOs is the only way to implement the FPP 8x without glue logic on the LS1043. The problem is that it will require for many GPIO pins.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信