Do the interfaces in the b4860qds support multicast?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Do the interfaces in the b4860qds support multicast?

562 次查看
victorgomez
Contributor II

Hi There!

I am running into problems when using multicast in two different b4860qds boards Do these boards support multicast at all?

Thanks!

0 项奖励
回复
1 回复

518 次查看
bpe
NXP Employee
NXP Employee

Yes, multicast is supported by DPAA, there are no known issues with hardware or software:

Submit Form


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复