CodeWarrior tool for QorIQ T-Series PowerPc Architecture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior tool for QorIQ T-Series PowerPc Architecture

Jump to solution
753 Views
Arathi
Contributor II

Hi NXP Support Team,

I am having QorIQ T2080 processor and I am using Code Warrior for PowerPC architecture Tool version 10.5.1 .

I am not sure whether this is the latest CodeWarrior for PowerPC architecture because I am unable to find some RCW values

For eg in Hardcoded value for cfg_rcw_src[0:8] :9’b0_1001_111x (Table 4-16 of T2080RM) 
MEM_PLL_RAT is 11:1 but in CW tool 11:1 ratio is not found.
CGA_PLL1_RAT is 7:1 but option not found in tool 
Attaching the same for your reference

Can you please let me know if this is the correct and latest version to be used for T2080 Processor.

Arathi_0-1696682599063.png

Arathi_5-1696683302473.png

 

Arathi_3-1696683200970.png

 

Arathi_2-1696682808241.png

Thanks and Regards,
Arathi

0 Kudos
1 Solution
694 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please type "11" then click "Apply", please refer to my screenshot.

yipingwang_0-1696908627138.png

 

 

View solution in original post

4 Replies
717 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to "Table 4-14. RCW Field Descriptions" for proper MEM_PLL_RAT and CGA_PLL1_RAT configuration in your RCW.

If you insist to use your custom value, you could use this method, please click the drop down icon in properties panel, then check "Ignore Constraints and non-Critical Errors".

Then double click MEM_PLL_RAT and add the "Custom Bitfield Value".

yipingwang_0-1696756362861.png

 

0 Kudos
707 Views
Arathi
Contributor II

Hi @yipingwang ,

I have tried the steps as mentioned by you.
Attaching the error results obtained for the same 

Arathi_0-1696839314617.png

Thanks,
Arathi

0 Kudos
695 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please type "11" then click "Apply", please refer to my screenshot.

yipingwang_0-1696908627138.png

 

 

661 Views
Arathi
Contributor II

Hi @yipingwang ,

Thanks for your reply.

After selecting Ignore Constraints and non-critical errors I was able to configure with my custom value as shown in the screenshot below

Arathi_0-1697203597459.png

Thanks and Regards,
Arathi

0 Kudos