Table 4-16 cfg_rcw_src[0:8] -> 0x9A or 0x9E or 0x9F.
When does set this cfg_rcw_src?
Do this matter for Nor boot or SD boot?
We will think so that following cfg_rcw_src setting for SD boot.
cfg_rcw_src[0:8] = 0x40
Table 4-16. RCW Settings for hard-coded RCW options.
If there is no valid RCW on the target bard, you need to configure the target board as hard-coded RCW, then use CodeWarrior to connect to the target board to do flash programming. Hard-coded RCW has no relation with Nor boot or SD boot.
Thank you for your reply.
I understand the content.
I will check with CodeWarrior.