Hi,
I got this error and the only info that I have is
Description Resource Path Location Type
Property DDR_RATE is set to a custom value. LS2088ARDB-Ben1 PBL1 Problem
It is not very usefull.
I pass every section in Properties page but I did not find any custom value.
I attached the PBL binary file. Note I add .c to be able to upload it but it's a binary file.
Thanks
已解决! 转到解答。
1.From Component Inspector view, select Enable/disable error checking menu, and then choose Skip error checking option, as shown in the figure below.